Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:tools-software:sigmastudio:toolbox:systemschematicdesign:hierarchyboard [19 Jun 2012 17:21] – created William Jahnresources:tools-software:sigmastudio:toolbox:systemschematicdesign:hierarchyboard [29 Jul 2020 05:18] (current) – Dummy save to fix version control Joshua Berlin
Line 6: Line 6:
 Schematic Hierarchy Boards allows you to create multiple layers within the schematic design window, providing additional schematic workspace. Hierarchy Boards are helpful for large schematic designs and for organizing design components. Hierarchy boards support Copy/Paste, schematic settings, and Undo operations.  In addition Hierarchy boards can be saved to files to create reusable design components. Schematic Hierarchy Boards allows you to create multiple layers within the schematic design window, providing additional schematic workspace. Hierarchy Boards are helpful for large schematic designs and for organizing design components. Hierarchy boards support Copy/Paste, schematic settings, and Undo operations.  In addition Hierarchy boards can be saved to files to create reusable design components.
  
- +  
  
  
Line 18: Line 18:
   * Drag a Hierarchy Board block into the workspace. It will have no input or output pins.   * Drag a Hierarchy Board block into the workspace. It will have no input or output pins.
   * The board block is associated with a Hierarchy Tab located at the bottom of the Schematic design window. The default name is Board1, the corresponding tab will have the same name as the board block. \\ {{hierarchyboardpic1.png}}   * The board block is associated with a Hierarchy Tab located at the bottom of the Schematic design window. The default name is Board1, the corresponding tab will have the same name as the board block. \\ {{hierarchyboardpic1.png}}
-  * The Hierarchy Board block provides an interface to route signals in our out of a Hierarchy board layer. To route signals into or out of the board, input and output pins must be created. See Hierarchy Input and Hierarchy Output for more information.+  * The Hierarchy Board block provides an interface to route signals in our out of a Hierarchy board layer. To route signals into or out of the board, input and output pins must be created. See [[resources/tools-software/sigmastudio/toolbox/systemschematicdesign/hierarchyinput|Hierarchy Input]] and [[resources/tools-software/sigmastudio/toolbox/systemschematicdesign/hierarchyoutput|Hierarchy Output]] for more information.
    
  
Line 30: Line 30:
    
    
-See the Hierarchy Board [[resources/tools-software/sigmastudio/toolbox/examples|System Example]] for a sample hierarchy board design.+See the Hierarchy Board [[resources/tools-software/sigmastudio/tutorials/systemexamples|System Example]] for a sample hierarchy board design.
    
  
resources/tools-software/sigmastudio/toolbox/systemschematicdesign/hierarchyboard.1340119319.txt.gz · Last modified: 19 Jun 2012 17:21 by William Jahn