Wiki

This version (02 Aug 2012 20:59) was approved by Brett Gildersleeve.The Previously approved version (02 Aug 2012 16:30) is available.Diff

Triangle Wave

Click here to return to the Sources section.

The Triangle Wave block generates a triangle wave at a constant level and frequency. The output frequency is adjustable. Use the edit control or arrows to set the desired frequency; the checkbox control turns the signal on and off.



To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz).

Note: The triangle wave is digitally generated and is non-bandlimited. This waveform is suitable for use as an internal control signal, but will produce aliasing distortion if used directly for audio output. If this configuration is desired, it is recommended that you apply a low-pass filter to the block's output before routing the signal to hardware outputs.

resources/tools-software/sigmastudio/toolbox/sources/trianglewave.txt · Last modified: 02 Aug 2012 20:59 by Brett Gildersleeve