Click here to return to the Sources section.
The Sawtooth Wave block generates a sawtooth wave (or saw wave) at a constant level and frequency. The output frequency is adjustable. Use the edit control or arrows to set the desired frequency; the checkbox control turns the signal on and off.. The gain and the initial phase of the algorithm can be configured.
To change the source's Sampling Rate, Right-click in the block and select Set Sampling Rate, which will open the Sampling Rate window (default is 44.1 kHz).
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
on/off | off | on/off | Turns the output of the cell on or off. When the output is off, the output pin will output a constant value of 0. |
Frequency | 500.01 | 0.01 to 0.5*Sample Rate | The sets the frequency of the sawtooth that is output from the cell. |
Initial Phase | 0 | 0 to 360 | Initial Phase of the sawtooth signal. |
Gain | 0 | -144 to 42 dB / -134 to 24 db | The gain to be multiplied on the sawtooth wave |
This module can be grown to support multiple phase/gain values for a single sawtooth wave.