The information here is preliminary.
Click here to return to the SigmaStudio Algorithm Resource Summary section.
Category | Algorithm | Executed Instructions | Program RAM | DATA Ram | Parameter RAM | Description | Processors | ||
---|---|---|---|---|---|---|---|---|---|
Clippers | Advanced Clip | 63 | 63 | 9 | 31 | Clips the input signal in an intelligent way when the signal exceeds a threshold. | ADAU144x, ADAU176x, ADAU1781 | ||
Clippers | Advanced Clip (Grow) | 63 | 63 | 1 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 | ||
Clippers | Standard Cubic | 21 | 21 | 3 | 5 | Soft clipper that uses a cubic function to clip the level of the input signal. | ADAU144x, ADAU176x, ADAU1781 | ||
Clippers | Standard Cubic (Grow) | 21 | 21 | 1 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 | ||
Clippers | Data Controlled Clip | 10 | 10 | 1 | 0 | Hard-clipper that clips the input data signal according to threshold values set by data input pins. | ADAU144x, ADAU176x, ADAU1781 | ||
Clippers | Data Controlled Clip (Grow) | 10 | 10 | 1 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 | ||
Clippers | Standard Clip | 7 | 7 | 1 | 1 | Clips off portions of signal voltages above and/or below certain limits. In other words, the circuit limits the range of the output signal. | ADAU144x, ADAU176x, ADAU1781 | ||
Clippers | Standard Clip (Grow) | 5 | 5 | 1 | 0 | Adds another channel to the block. | ADAU144x, ADAU176x, ADAU1781 |