This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudio:toolbox:licensedalgorithms:hdsx [20 Aug 2013 14:04] – [Now available as a free Trial version: HDSX® - High Definition Sound Expansion] Gunnar Kron | resources:tools-software:sigmastudio:toolbox:licensedalgorithms:hdsx [17 Sep 2020 11:28] (current) – Gunnar Kron | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
[[resources/ | [[resources/ | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | This block is included in the SigmaStudio installation | + | These blocks are not included in the SigmaStudio installation. Please contact |
</ | </ | ||
- | HDSX® - High Definition Sound Expansion increases the sound quality, especially of little- and small-field positioned sound sources by expanding the sound field and the spatial hearing experience in a very unique way. It creates a new quality of small speaker entertainment like used in mobile devices, flatscreen TV's, headphones, gaming- and automotive solutions. | + | <WRAP center round important 60%> |
+ | Decoders, running on DSPs with at least four channel input, can also be delivered as automotive versions with 2x2.0 input (Front/ | ||
+ | </ | ||
+ | |||
+ | ===== HDSX Surround 2.0 - 5.0/5.1 RealCenter® ===== | ||
+ | **Available on ADAU 1452 and others on request** | ||
+ | |||
+ | RealCenter technology for precise center extraction and localization. TruDirection® Surround channels for enhanced directional localization. Decoded output channels: L, | ||
+ | |||
+ | ===== HDSX Surround 2.0 - 7.0/7.1 RealCenter ===== | ||
+ | **Available on ADAU 1452 and others on request** | ||
+ | |||
+ | RealCenter technology for precise center extraction and localization. TruDirection® Surround channels for enhanced directional localization. Decoded output channels: L, | ||
+ | |||
+ | ===== HDSX Surround 2.0 - 5.0/5.1 LowMips ===== | ||
+ | **Available on ADAU 1452, ADAU 144x, ADAU 1701 and others on request** | ||
+ | |||
+ | L+R Center Channel. TruDirection® Surround channels for enhanced directional localization. Decoded output channels: L, | ||
+ | |||
+ | ===== HDSX Virtual Center | Speech enhancer ===== | ||
+ | |||
+ | **Available on ADAU 1452 and others on request** | ||
+ | |||
+ | This block enables independent volume control of the phantom center within stereo sources. It is not a hidden L+R upmix. A crossover frequency can be set to split the phantom center. | ||
+ | |||
+ | **Available on ADAU 1452 and others on request** | ||
+ | |||
+ | ===== HDSX Stereo Sound Widening 360 ===== | ||
+ | **Available on SigmaDSP 100, | ||
+ | |||
+ | HDSX® - High Definition Sound Expansion increases the sound field, especially of little- and small-field positioned sound sources by expanding the sound field and the spatial hearing experience in a very unique way. It creates a new spatial | ||
- | For details, please visit www.kronoton.com. | + | More infos under www.hdsx.audio. |
- | ===== Example | + | **Example |
A schematic, with the input block, the easy to use HDSX® plug in and the output block, is shown below. | A schematic, with the input block, the easy to use HDSX® plug in and the output block, is shown below. |