Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

resources:tools-software:sigmastudio:toolbox:io:spdifinputoutput [21 Jun 2012 21:04] – created Brett Gildersleeveresources:tools-software:sigmastudio:toolbox:io:spdifinputoutput [06 Aug 2012 22:45] (current) – created Brett Gildersleeve
Line 1: Line 1:
-<WRAP center round todo 60%> +====== SPDIF Input/Output ======
-Under Construction +
-</WRAP>+
  
 +[[resources:tools-software:sigmastudio:toolbox:io|Click here to return to the Inputs and Outputs Toolbox page.]]
 +
 +{{ :resources:tools-software:sigmastudio:toolbox:io:spdif_io_012.jpg?|}}
 +
 +The SPDIF Input and Output blocks route signals between the schematic design and the hardwares's SPDIF pins.
 +
 +Use the input block's check boxes to enable or disable an input. Use the output block's drop-down list control to select from the available SPDIF outputs.
 +
 +Every enabled input must be connected to an output, else there will be errors on compilation.
 +
 +To change the SPDIF Input block's Sampling Rate , Right-click the block name and select Set Sampling Rate, which brings up the Sampling Rate window (default is 44.1 kHz).
 +
 +<WRAP center round info 60%>
 +Note: These blocks are only available for use with DSPs that have SPDIF I/O.
 +</WRAP>
resources/tools-software/sigmastudio/toolbox/io/spdifinputoutput.txt · Last modified: 06 Aug 2012 22:45 by Brett Gildersleeve