Click here to return to the Inputs and Outputs Toolbox page.
The SPDIF Input and Output blocks route signals between the schematic design and the hardwares's SPDIF pins.
Use the input block's check boxes to enable or disable an input. Use the output block's drop-down list control to select from the available SPDIF outputs.
Every enabled input must be connected to an output, else there will be errors on compilation.
To change the SPDIF Input block's Sampling Rate , Right-click the block name and select Set Sampling Rate, which brings up the Sampling Rate window (default is 44.1 kHz).
Note: These blocks are only available for use with DSPs that have SPDIF I/O.