This shows you the differences between two versions of the page.
resources:tools-software:sigmastudio:toolbox:io:generalpurposeinput [21 Jun 2012 21:04] – created Brett Gildersleeve | resources:tools-software:sigmastudio:toolbox:io:generalpurposeinput [06 Aug 2012 22:51] (current) – created Brett Gildersleeve | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | <WRAP center round todo 60%> | + | ====== General-Purpose Input ====== |
- | Under Construction | + | |
+ | [[resources: | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | The General Purpose Input block allows signals from the hardware' | ||
+ | |||
+ | There are 12 selectable inputs to this GPIO block. | ||
+ | |||
+ | <WRAP center round info 60%> | ||
+ | Note: The block is only available for DSPs that include GPIO. To configure the hardware' | ||
</ | </ | ||
+ | Select the channel desired for sending your signal using the General Purpose Input drop-down control. | ||
+ | |||
+ | * Every enabled input must be connected to an output, else there will be errors on compilation. | ||
+ | * Observe that as you drag more output blocks to your schematic, your number of input channels available in the drop-down decreases. | ||
+ | * To change the Sampling Rate for the Input, Right-click the block name and select Set Sampling Rate, which brings up the Sampling Rate window (default is 44.1 kHz): | ||
+ | |||
+ | {{ : |