Click here to return to the Inputs and Outputs Toolbox page.
The General Purpose Input block allows signals from the hardware's GPIO input pins to be used in a schmeatic design. The orange output pin should typcially be connected to a GPIO Conditioning block.
There are 12 selectable inputs to this GPIO block.
Note: The block is only available for DSPs that include GPIO. To configure the hardware's GPIO input and outputs settings, see the processors Register Control Window.
Select the channel desired for sending your signal using the General Purpose Input drop-down control.