Click here to return to the Dynamics Processors page
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Audio Input L | decimal - audio | Left Channel audio input |
Pin 1: Audio Input R | decimal - audio | Right Channel audio input |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Audio Output L | decimal - audio | Left Channel compressed Audio Output |
Pin 0: Audio Output R | decimal - audio | Right Channel compressed Audio Output |
*The GUI Controls for this block exist on another window. Click on the Compressor icon to open the following Compressor window that contains the following Compressor controls:
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Threshold (dB) | 0 | -96 | Controls the threshold point of compression/expansion. |
Compressor | 100 | 100 - 1 | Controls the ratio of Compression. The number selected in this box is interpreted as the ratio N:1 for compression above the threshold point. |
Expander | 1 | 100 - 1 | Controls the ratio of Downward Expansion. The number selected in this box is interpreted as the ratio N:1 for downward expansion below the threshold point. |
Knee | 1 | 1 - 100 | Controls the hard/soft knee relationship of the curve. A knee allows a more gradual calculation of the curve around the threshold point, with “1” being a hard knee, and “100” being the softest. |
Input Gain (dB) | 0 | -96 | Controls a gain that is applied to both Left and Right prior to the compression. Allows for the curve to be shifted left and right. |
Attack (ms) | 72 | 1- 500 | Controls the amount of time before the compressor reacts to an input signal that has exceeded the threshold point. |
Hold (ms) | 0 | 0 - Attack | Controls the amount of time the compression level is held before reacting to a new change in input signal level. The max hold time is limited to the Attack time setting. |
Release (ms) | 868 | Jan-00 | Controls the amount of time before the compressor reacts to an input signal that has dropped below the threshold point. |
Level Indicators | off | on/off | Turns the Indicators on or off. There is no DSP function associated with this. |
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Threshold Compressor Expander Knee | StdPeakCompressorAlg1 | When the Threshold, Compressor, Expander, or Knee values are changed, 34 parameters are written to the DSP to represent the gain curve displayed in the window. |
Input Gain | StdPeakCompressorAlg1attenuation | When the Input Gain is changed, the dB value is converted to linear and written to the DSP. |
Attack | StdPeakCompressorAlg1Peak | When the Attack time is changed, a new value is calculated and written to the DSP to control the reaction time. |
Hold | StdPeakCompressorAlg1hold | When the Hold time is changed, a new value is calculated and written tot he DSP to control the hold time. |
Decay | StdPeakCompressorAlg1decay | When the Decay time is changed, a new value is calculated and written to the DSP to control the reaction time. |
The Standard RMS Compressor is meant to function like most other SigmaStudio compressors. The performance and main algorithm driving the Standard RMS is the same as the other compressors in the same library folder (RMS - Standard Resolution - Lower Range). The main differences are outlined here:
*The Standard RMS Compressor is a stereo compressor with the detection method tied directly to the inputs. Thus the detection signal used to drive the compression is: Input Gain * (L + R)/2. There is no choice for an external signal to drive the compression. This detection method is the same as selecting “No External Detection” on other compressors in the same library folder.
If independent control of the detection method is desired for compression, the Standard Independent RMS compressor should be used. This allows different functionality to link or unlink the detection method for left and right channels.
This is an example of the compressor being used directly on the input signal. The compressor is connected to an external Volume Control for a post gain level before sending to the outputs.
Toolbox Path | RMS - Standard Resolution - Lower Range - Standard RMS |
Cores Supported | ADAU144x ADAU176x \\ADAU178x |
“Grow Algorithm” Supported | no |
“Add Algorithm” Supported | no |
Subroutine/Loop Based | no |
Program RAM | 64 |
Data RAM | 20 |
Parameter RAM | 45 |