Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Input | any - any | Input signal that is monitored for the first rising edge |
Name | Format [int/dec] - [control/audio] | Function Description |
---|---|---|
Pin 0: Trigger | any - control | Output flag signal set to “1” in the selected bit position |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Output Bit Designation | 28 | [28.0 Bit26] | Sets bit position of the output “1” flag. 28.0 is the default values which represents 1LSB. |
GUI Control Name | Compiler Name | Function Description |
---|---|---|
Output Bit Designation | OneShotFallAlg1output1 | Actual value written to DSP from the representation of the drop-down menu to select the bit position of the output “1” flag. |
The following graph shows the output response based on a given input signal through the One Shot Rise block. There are two different case scenarios:
Case1: The input signal starts high
Case2: The input signal starts low
In the graphs the input signal is only toggling between “1” and “0” however this algorithm will respond to any changes in level of the input signal, thus the first rising edge of the input signal will trigger the output to go high.
The format of the “1” output value of the is designated by the drop-down menu. The following table shows the “1” Output that corresponds to the drop-down menu selection.
The following image shows the OneShot Rise block being used. A switch source is connected to the input and then the output of the block is driving a GPIO output. When the switch is clicked “high” the signal sent to the GPIO output will be “high.”
Toolbox Path | Basic DSP - Logic - Toggle - OneShot rise |
Cores Supported | AD1940 ADAU170x ADAU144x ADAU176x ADAU178x |
“Grow Algorithm” Supported | no |
“Add Algorithm” Supported | no |
Subroutine/Loop Based | no |
Program RAM | 5 |
Data RAM | 4 |
Parameter RAM | 1 |