Click here to return to the Basic DSP section.
This module can be used to read any parameter/array of parameter values from schematic. Also it can write the read values to the file periodically.
None
None
The module currently does not support grow/add functionality.
The DSP param readback module contains controls to initiate single read/continuous read.
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Read Button | - | - | Click on this button to initiate single read. |
Continuous Read Circle | - | - | Click on this circle to initiate continious read. This will be visible only if the continuous read is enabled in the readback configuration |
After Link Compile Download right click on the module then select 'Configure…' to configure the parameter read options. After configuring, press read button/continuous read circle to initiate the read.
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
Block Name | - | All the modules name in the current schematic | Lists all the modules in the current schematic. |
Parameter Name | - | All the parameter in the module selected in 'Block Name' field. | Lists all the parameter in the module selected in 'Block Name' field. |
Address Enable Checkbox | Not Checked | Checked/Not Checked | Enables the address field editable. When address field is editable 'Block Name' and 'Parameter Name' fields can not be edited. |
Address | - | - | Address from which the data to be read from the target. |
Parameter Length | 1 | 1-65536 | Number of values to be read from the parameter Address. |
Enable Continuous Read Back Checkbox | Not Checked | Checked/Not Checked | Enables the continuous readback button in the module |
Readback Period | 500 ms | 500 - 2000 ms | Period at which read back to be initiated in continuous reaback mode |
Output File Enable Checkbox | Not Checked | Checked/Not Checked | Enables the output file write option. |
Output File | - | - | File to which the data to be written. |
File Write Duration | 1 | 1-5 | Duration for which file write operation occurs. |
Notes: