This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudio:toolbox:adialgorithms:adisurround [14 Nov 2012 19:41] – Initial Content added William Jahn | resources:tools-software:sigmastudio:toolbox:adialgorithms:adisurround [19 Jan 2017 21:50] (current) – Added detail about the "room" sizes. David Thibodeau | ||
---|---|---|---|
Line 22: | Line 22: | ||
* Size1 = small | * Size1 = small | ||
* Size2 = large | * Size2 = large | ||
+ | These Large and Small settings are to make it sound like a small or large room. This is a setting that can be experimented with to adjust for the room the system is in and personal preference. So there is no " | ||
The schematic shown below features an input block (two-channel), | The schematic shown below features an input block (two-channel), | ||
{{ : | {{ : |