Wiki

This version is outdated by a newer approved version.DiffThis version (14 Nov 2012 19:49) was approved by William Jahn.The Previously approved version (05 Nov 2012 20:08) is available.Diff

This is an old revision of the document!


ADI Surround

Click here to return to the ADI Algorithms page

ADI Surround uses matrix-surround decoding techniques: deriving five channels of output from a two-channel input. This process entails using a sum channel (the combination of the left and right channels, L+R), which contains frontal information, and a difference channel (the difference between the left and right channels, L-R / R-L), which contains ambiance information.

Depending on the blending and distribution of the difference channel with the sum channel, we can derive the left, right, center, and side or rear surround channels. The L and R front speakers carry music, frontal sound effects, and directional dialog; the center speaker carries the rest (meaning most) of the dialog, and the surround speakers (ideally placed to the side of and slightly above the listeners) provide ambiance and surround effects.

ADI Surround has presets for the following modes:

  • Club
  • Music
  • Stadium
  • Cinema
  • Hall
  • Rock
  • Jazz
  • User1
  • User2
  • User3

It also features two room sizes:

  • Size1 = small
  • Size2 = large

The schematic shown below features an input block (two-channel), ADI Surround (configuration = Club, size = small) and output blocks.

resources/tools-software/sigmastudio/toolbox/adialgorithms/adisurround.1352918460.txt.gz · Last modified: 14 Nov 2012 19:41 by William Jahn