This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:tools-software:sigmastudio:toolbox:adialgorithms:adisurround [05 Nov 2012 20:08] – created William Jahn | resources:tools-software:sigmastudio:toolbox:adialgorithms:adisurround [14 Nov 2012 19:41] – Initial Content added William Jahn | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADI Surround ====== | ====== ADI Surround ====== | ||
- | ------------------------------------------------------------------------------------------------- | ||
- | <WRAP center round todo 60%> | + | [[resources/tools-software/ |
- | This page is under construction | + | |
- | </WRAP> | + | |
+ | ADI Surround uses matrix-surround decoding techniques: deriving five channels of output from a two-channel input. This process entails using a sum channel (the combination of the left and right channels, L+R), which contains frontal information, | ||
+ | |||
+ | Depending on the blending and distribution of the difference channel with the sum channel, we can derive the left, right, center, and side or rear surround channels. The L and R front speakers carry music, frontal sound effects, and directional dialog; the center speaker carries the rest (meaning most) of the dialog, and the surround speakers (ideally placed to the side of and slightly above the listeners) provide ambiance and surround effects. | ||
+ | |||
+ | ADI Surround has presets for the following modes: | ||
+ | * Club | ||
+ | * Music | ||
+ | * Stadium | ||
+ | * Cinema | ||
+ | * Hall | ||
+ | * Rock | ||
+ | * Jazz | ||
+ | * User1 | ||
+ | * User2 | ||
+ | * User3 | ||
+ | |||
+ | It also features two room sizes: | ||
+ | * Size1 = small | ||
+ | * Size2 = large | ||
+ | |||
+ | The schematic shown below features an input block (two-channel), | ||
+ | |||
+ | {{ : |