This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:sigmastudio:developmentenvironment:workspacewindows [14 Jun 2012 23:06] – Added parameters section, under construction, and video link Brett Gildersleeve | resources:tools-software:sigmastudio:developmentenvironment:workspacewindows [28 Apr 2015 17:18] (current) – [Sequence Window:] John McCarty | ||
---|---|---|---|
Line 33: | Line 33: | ||
\\ | \\ | ||
- | <note tip> | + | <WRAP tip> |
- | </note> | + | </WRAP> |
-------------------------------------------------------------------------------- | -------------------------------------------------------------------------------- | ||
Line 48: | Line 48: | ||
\\ | \\ | ||
- | <note tip> | + | <WRAP tip> |
See Capture Output Data for a detailed explanation of the data displayed in the Capture Window. | See Capture Output Data for a detailed explanation of the data displayed in the Capture Window. | ||
Line 58: | Line 58: | ||
<WRAP todo> | <WRAP todo> | ||
- | <note tip> | + | <WRAP tip> |
-------------------------------------------------------------------------------- | -------------------------------------------------------------------------------- | ||
====Sequence Window:==== | ====Sequence Window:==== | ||
+ | Use the sequence window to define a custom sequence of data read/write operations between SigmaStudio and a target hardware device connected via USB. Commands can be dragged from the capture window or created manually. | ||
+ | \\ | ||
- | <WRAP todo> | + | The sequence window is part of the Capture window, to view the sequence window open the capture window and click the arrow button in the upper right corner. |
+ | |||
+ | {{: | ||
+ | |||
+ | {{: | ||
+ | \\ | ||
+ | \\ | ||
+ | |||
+ | === Define a sequence === | ||
+ | |||
+ | 1. Drag and drop data directly from the capture window. | ||
+ | {{: | ||
+ | |||
+ | 2. Right-click in the sequence window to define an operation manually. | ||
+ | {{: | ||
+ | \\ | ||
+ | \\ | ||
+ | |||
+ | === Execute a sequence === | ||
+ | Click the download Mode to Hardware button to execute sequence commands. | ||
+ | {{: |