Wiki

This version is outdated by a newer approved version.DiffThis version (14 Jun 2012 23:06) was approved by Brett Gildersleeve.The Previously approved version (14 Jun 2012 23:04) is available.Diff

This is an old revision of the document!


Workspace Windows

Click here to return to the Development Environment page

The Workspace windows display important project information including available resources, compiler output, and hardware communication. To show or hide the workspace windows select them in the application's main View menu or by clicking the buttons on the Standard Toolbar.

  • DSP Resources
  • Output
  • Capture Window
  • Sequence Window

Each window is described below:


DSP Resources:

The DSP Resources window lets you view the resources available in your design, depending on your project complexity. You are able to monitor program RAM, parameter RAM, and other hardware-specific resources. By default this window is docked on the right side of the program window.



Output:

The Output window is a quick way to view the files generated upon linking, compiling, and other actions in the Schematic workspace. By default this window is docked on the right side of the program window. Note, you can also find this information by locating the project's output folder and reading the compiler output files. For more information about those files, see Compile/Downloading Your Project.


Note: The DSP Resources and Output windows are not fully functional for all SigmaDSP IC types.

Capture Window:

The capture window lets you see, in real time, the exact data that SigmaStudio is sending to the hardware. This window is only active when a USB communication channel is inserted in the project and the project has been compiled and downloaded. This window is un-docked/floating by default.

The window is empty when it opens initially, but after you press Link-Compile-Download you will see the data that is downloaded to the board: coefficients, parameter addresses, and parameter data. Whenever you make adjustments to sliders or control in a compiled and downloaded schematic, you can see the data that is sent.


See Capture Output Data for a detailed explanation of the data displayed in the Capture Window.


Parameters Window:

Under Construction


Sequence Window:

Under Construction

resources/tools-software/sigmastudio/developmentenvironment/workspacewindows.1339707991.txt.gz · Last modified: 14 Jun 2012 23:06 by Brett Gildersleeve