The SHARC Audio Module uses the ADSP-SC589 SHARC processor along with an ADAU1761 SigmaDSP audio codec and an AD2425W A2B transceiver in a compact form for audio development.
The SHARC Audio Module Main Board
Block Diagram of the SHARC Audio Module Main Board
SHARC Audio Module Main Board Rev 1.4 Design and Integration Files
The SHARC Audio Module is powered by the Analog Devices, Inc. ADSP-SC589 SHARC DSP. The ADSP-SC589 contains an ARM Cortex-A5 and Dual SHARC+ cores running at 450 MHz.
There are two DDR3 channels on the SHARC Audio Module, each with a 2Gbit DDR3 module. In the default SHARC Audio Module configuration, one DDR3 module is used for Linux and the other used by the SHARC+ cores for audio processing.
A 512Mbit SPI Flash on the SHARC Audio Module that is ready to be programmed with a users desired audio application.
The SHARC Audio Module has a 10/100/1000 Ethernet module to provide network and internet access to the board. The default IP address for this board, while running the official SHARC Audio Module Linux OS is 192.168.1.9.
The USB Type A port is Host mode only, and is for USB WiFi, Bluetooth and USB memory devices.
The USB MicroAB can be a Host/Device or OTG connection. This interface can be used for USB Audio, along with the USBi Emulator.
+12v | 1 | 2 | +12v |
GND | 3 | 4 | GND |
TWI1_SCL | 5 | 6 | PB_00 |
TWI1_SDA | 7 | 8 | PB_01 |
GND | 9 | 10 | PB_02 |
DAI0_PIN13 | 11 | 12 | PB_03 |
DAI0_PIN14 | 13 | 14 | GND |
DAI0_PIN15 | 15 | 16 | PB_04 |
GND | 17 | 18 | PB_05 |
DAI0_PIN16 | 19 | 20 | PD_14 |
DAI0_PIN17 | 21 | 22 | PD_15 |
DAI0_PIN18 | 23 | 24 | GND |
+3.3v | 25 | 26 | PE_00 |
GND | 27 | 28 | PE_01 |
HADC0_VIN0 | 29 | 30 | PE_02 |
HADC0_VIN1 | 31 | 32 | PE_03 |
GND | 33 | 34 | GND |
HADC0_VIN2 | 35 | 36 | PE_04 |
HADCO_VIN3 | 37 | 38 | PE_05 |
GND | 39 | 40 | PE_06 |
HADC0_VIN4 | 41 | 42 | PE_07 |
HADC0_VIN5 | 43 | 44 | PE_08 |
GND | 45 | 46 | GND |
HADC0_VIN6 | 47 | 48 | PE_09 |
HADC0_VIN7 | 49 | 50 | PE_10 |
GND | 51 | 52 | PE_11/SPI1_SEL3 |
PD_12/UART2_TX | 53 | 54 | PE_12/SPI1_SEL4 |
PD_13/UART2_RX | 55 | 56 | PE_13/SPI1_CLK |
TWI2_SCL | 57 | 58 | PE_14/SPI1_MISO |
TWI2_SDA | 49 | 60 | PE_15/SPI1_MOSI |
PB_11 | 61 | 62 | PB_13 |
PB_12 | 63 | 64 | PB_14 |
DAI1_PIN01 | 1 | 2 | DAI1_PIN11 |
DAI1_PIN02 | 3 | 4 | DAI1_PIN12 |
DAI1_PIN03 | 5 | 6 | DAI1_PIN13 |
GND | 7 | 8 | GND |
DAI1_PIN04 | 9 | 10 | DAI1_PIN14 |
DAI1_PIN05 | 11 | 12 | DAI1_PIN15 |
DAI1_PIN06 | 13 | 14 | DAI1_PIN16 |
GND | 15 | 16 | GND |
DAI1_PIN07 | 17 | 18 | DAI1_PINI17 |
DAI1_PIN08 | 19 | 20 | DAI1_PIN18 |
DAI1_PIN09 | 21 | 22 | DAI1_PIN19 |
DAI1_PIN10 | 23 | 24 | DAI1_PIN20 |
GND | 25 | 26 | GND |
PD_04 | 27 | 28 | PD_06 |
PD_05 | 29 | 30 | PD_07 |
PC_07/CAN0_RX | 31 | 32 | PB_09/CAN1_TX |
PC_08/CAN0_TX | 33 | 34 | PB_10/CAN1_RX |
PC_09/SPI0_CLK | 35 | 36 | PC_00 |
PC_10/SPI0_MISO | 37 | 38 | PB_15 |
PC_11/SPI1_MOSI | 39 | 40 | GND |
PC_12/SPI1_SEL3 | 41 | 42 | +3.3v |
PG_00 | 43 | 44 | PF_14 |
PG_01 | 45 | 46 | PF_15 |
PG_02 | 47 | 48 | PG_03 |
TWI0_SCL | 49 | 50 | PG_04 |
TWI0_SDA | 51 | 52 | PG_05 |
GND | 53 | 54 | GND |
ADAU1761_RAUX | 55 | 56 | ADAU1761_RHP |
GND | 57 | 58 | GND |
ADAU1761_LAUX | 49 | 60 | ADAU1761_LHP |
PD_08 | 61 | 62 | PD_10 |
PD_09 | 63 | 64 | PD_11 |
This connector is compatible with most FTDI 3.3v UART to USB adapters.
1 | GND |
2 | PD_00/UART0_CTS |
3 | N/C |
4 | PC_14/UART0_RX |
5 | PC_13/UART0_TX |
6 | PC_15/UART0_RTS |
The A2B bus uses crossover cables to connect nodes to each other. P6
connects to
upstream towards the Master Node in the network and P7
connects downstream to
the next slave in the network. The SHARC Audio Module uses the AD2425W IC.
BLCK
is connected to DAI0_PIN07
SYNC
is connected to DAI0_PIN08
DTX0
is connected to DAI0_PIN09
DTX1
is connected to DAI0_PIN10
DRX0
is connected to DAI0_PIN11
DRX1
is connected to DAI0_PIN12
The ADAU1761 is a low power, stereo audio codec with integrated digital audio processing that supports stereo 48 kHz record and playback. The stereo audio ADCs and DACs support sample rates from 8 kHz to 96 kHz as well as a digital volume control.
The SigmaDSP® core features 28-bit processing (56-bit double precision). The processor allows system designers to compensate for the real-world limitations of microphones, speakers, amplifiers, and listening environments, resulting in a dramatic improvement in the perceived audio quality through equalization, multiband compression, limiting, and third-party branded algorithms.
The ADAU1761 is connected to the DAI ports on the ADSP-SC589 as follows:
DAC_SDATA
is connected to DAI0_PIN01
ADC_SDATA
is connected to DAI0_PIN02
BCLK
is connected to DAI0_PIN03
LRCLK
is connected to DAI0_PIN04
The 3.5mm Audio In/Out jacks are connected to the ADAU1761 SigmaDSP.
The impedance of the 3.5mm signals is 16 ohms. The HP output pins to the expansion connectors are also 16 ohms.
The SPDIF jacks are connected to the DAI ports on the ADSP-SC589.
DAI0_PIN19
.DAI0_PIN20
.The USBi Connector on the SHARC Audio module allows for the use of the USBi adapter for bare metal programming.
The SHARC Audio Module was design for a 12V DC input, but can operated from 10v to 20v input to the barrel jack. A 12v 1.5A DC power supply is recommended. The barrel connector on the SHARC Audio Module can handle up to 3A current.
The SHARC Audio Module is shipped with a US power supply. Here is a universal option: https://www.digikey.com/products/en?keywords=102-3580-ND
The MicroSD card slot on the SHARC Audio Module can be used to store the Linux OS as well as other data.
The JTAG interface allows for programming and debugging of the ADSP-SC589 using an ICE-1000 or an ICE-2000 emulator and CrossCore Embedded Studio.
The ADSP-SC589 has multiple boots modes. This jumper allows for three of the supported boot modes on the DSP, depending on jumper setting.
Jumper on Pins | Boot Mode |
---|---|
1-2 | SPI Boot |
2-3 | UART Boot |
None | No Boot |
SHARC Audio Module revisions 1.4 or older incorrectly use link port boot rather than UART boot
Two GPIO pushbuttons are provided on the SHARC Audio Model. They are connected as follows:
PB1
is connected to PF_00
PB2
is connected to PF_01
The Reset button resets all the hardware on the SHARC Audio Module. It will not reset anything on connected to the expansion connectors.
There are three GPIO controlled LEDs on the SHARC Audio Module. They are connected as follows:
LED10
is connected to PD_01
LED11
is connected to PD_02
LED12
is connected to PD_03
The SHARC Audio Module has a TWI switch the can connect TWI0 or TWI1 on the
ADSP-SC589 to the A2B and ADAU1761 on the board. This allows either the ARM core
or the SHARC+ cores to access the A2B and ADAU1761 TWI control lines. PB_08
controls the switch.
PB_08 | Connection |
---|---|
Low | TWI0 |
High | TWI1 |