This version (24 May 2021 17:58) was approved by Chad Wentworth.The Previously approved version (03 Mar 2020 17:47) is available.
This is an old revision of the document!
The SHARC Audio Module A2B Class-D Amplifier Module is an A2B connected board that contains two Class-D SSM3582 amplifier ICs, providing 4 channels of audio output.
The A2B Class-D Amplifier Module
Block Diagram of the A2B Class-D Amplifier Module
SHARC Audio Module A2B Class-D Amplifier Module Design and Integration Files
The A2B bus uses crossover cables to connect nodes to each other. P4 connects to upstream towards the Master Node in the network and P5 connects downstream to the next slave in the network.
The A2B Class-D Amplifier Module uses the AD2428W IC.
There are two ADI SSM3582 Class-D amplifiers on the A2B Class-D Amplifier Module. Each is two channels.
At 16V, the max power per channel is ~24w of power.
P11 AMP1 Left Channel Output
1 | Positive |
2 | Negative |
P12 AMP1 Right Channel Output/MONO
1 | Positive |
2 | Negative |
P13 AMP2 Left Channel Output
1 | Positive |
2 | Negative |
P14 AMP2 Right Channel Output/MONO
1 | Positive |
2 | Negative |
Populate JP6 & JP7 to configure AMP1 into MONO Output on P12.
Populate JP8 & JP9 to configure AMP2 into MONO Output on P14.
The USBi Connector on the SHARC Audio Module allows for the use of the USBi adapter for SigmaStudio and bare metal programming.
The A2B Class-D Amplifier Module is designed to run off a 12v to 16v supply. A 12v 2A DC power supply is included in the kit. The barrel connector on the A2B Class-D Amplifier Module can handle up to 3A current.
The Class-D Amplifier Module is shipped with a US power supply. Here is a universal option: https://www.digikey.com/products/en?keywords=102-3580-ND
P10 is a power supply input jack to connect up to 16v @ 8A MAX. There is an 8A fuse on the Positive input of the P10 connector.
Two GPIO pushbuttons are provided on the A2B Class-D Amplifier Module. They are connected as follows:
PB1 is connected to IO1 on AD2428WPB2 is connected to IO2 on AD2428WThere are two GPIO-controlled LEDs on the A2B Class-D Amplifier Module. They are connected as follows:
LED1 is connected to IO0 on the AD2428WLED2 is connected to IO7 on the AD2428WJP5 PDM MIC
| 3.3v | 1 | 2 | GND |
| DRX0 | 3 | 4 | GND |
| DRX1 | 5 | 6 | GND |
| BLCK | 7 | 8 | GND |
P2 Buffered TDM Signals
| B_DTX0 | 1 | 2 | GND |
| B_DTX1 | 3 | 4 | GND |
| B_DRX0 | 5 | 6 | GND |
| B_DRX1 | 7 | 8 | GND |
| B_FSYNC | 9 | 10 | GND |
| B_BLCK | 11 | 12 | GND |
P15 Unbuffered TDM Signals
| DTX0 | 1 | 2 | GND |
| DTX1 | 3 | 4 | GND |
| DRX0 | 5 | 6 | GND |
| DRX1 | 7 | 8 | GND |
| FSYNC | 9 | 10 | GND |
| BLCK | 11 | 12 | GND |
The A2B Class-D Amplifier Module has a TWI 256k EEPROM for configuration data. The EEPROM used is the 24FC256I/MS.