This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:sharc-audio-module:faust:ex-work-virtual-analog [03 Oct 2018 22:28] Chad Wentworth |
resources:tools-software:sharc-audio-module:faust:ex-work-virtual-analog [15 Nov 2018 15:01] Chad Wentworth [MIDI Virtual Analog Synth (Core1) /Effects (Core 2)] |
||
---|---|---|---|
Line 2: | Line 2: | ||
For this final example the full virtual analog synth is run on Core1 and the effects chain is run on Core 2. | For this final example the full virtual analog synth is run on Core1 and the effects chain is run on Core 2. | ||
- | <WRAP important> | + | <WRAP round important> |
- | Part of this example will run on core 2 so be sure to set the following #define in ''audio_system_config.h'' | + | Part of this example will run on core 2 so be sure to set the following #define in ''audio_system_config.h'' or select that Faust will run on both cores 1 and 2 when using the [[resources:tools-software:sharc-audio-module:baremetal:project-wizard|bare metal project wizard]]. |
<code c> | <code c> |