This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:sharc-audio-module:advanced-audio-projects:program-flash [22 May 2023 17:21] – Adding compatibility updates Rebecca Butler | resources:tools-software:sharc-audio-module:advanced-audio-projects:program-flash [22 May 2023 18:14] – CLPD Updates Rebecca Butler | ||
---|---|---|---|
Line 25: | Line 25: | ||
| 1. Power on your SAM board and plug in the 12V Power Supply to the 12V connector. If the board is properly powered, the green LED9/PWR will light up. | {{ : | | 1. Power on your SAM board and plug in the 12V Power Supply to the 12V connector. If the board is properly powered, the green LED9/PWR will light up. | {{ : | ||
| 2. Plug the USB Micro Type B side to the SAM board USB connector and the USB Type A side to a USB connection on the PC. | {{ : | | 2. Plug the USB Micro Type B side to the SAM board USB connector and the USB Type A side to a USB connection on the PC. | {{ : | ||
- | | 3. On the SAM board, press and hold buttons PB1 and PB2. While still holding PB1 and PB2, press RESET. \\ \\ //Note that you do not need to hold reset. Resetting the board while holding PB1 and PB2 down will tell the bootloader to stay in the bootloader and await instructions for application flash.// \\ \\ //If this is successful, LED10 will blink, while LED11 and LED12 will remain off.//| {{ : | + | | 3. On the SAM board, press and hold buttons PB1 and PB2. While still holding PB1 and PB2, press RESET. \\ \\ //Note that you do not need to hold reset. Resetting the board while holding PB1 and PB2 down will tell the bootloader to stay in the bootloader and await instructions for application |
| 4. Open the SAM Flasher Tool | {{ : | | 4. Open the SAM Flasher Tool | {{ : | ||
| 5. Select the //Comm Port// labelled //SC5xx Communications Port//. | {{ : | | 5. Select the //Comm Port// labelled //SC5xx Communications Port//. | {{ : | ||
Line 32: | Line 32: | ||
| 8. To enter the application, | | 8. To enter the application, | ||
- | ===== Application Flash via CLPD ===== | + | ===== Application Flash via CLPD via Bootswitch |
- | //TODO// | + | //Only available for products that support CLPD updates via Bootswitch!// |
+ | |||
+ | **Follow the instructions below for products which support CLPD updates via Bootswitch: | ||
+ | | 1. Set the bootswitch rotary switch to //0//. This tells the device to not automatically boot. | {{ : | ||
+ | | 2. Power on your board and plug in the 12V Power Supply to the 12V connector. If the board is properly powered, the green PWR LED will light up.\\ \\ //Location of LED will vary based on device.// | {{ : | ||
+ | | 3. Plug the ICE-1000 or ICE-2000 JTAG header into board header labelled //DEBUG//. Ensure that the USB-A connector is plugged into a USB-A receptacle on the PC and ensure the status of the debugger shows a green LED. | {{ : | ||
+ | | 4. Using Windows command prompt, navigate to //< | ||
+ | | 4. Open the SAM Flasher Tool | {{ : | ||
+ | | 5. Select the //Comm Port// labelled //SC5xx Communications Port//. | {{ : | ||
+ | | 6. Select //Load// and navigate to the LDR that was [[: | ||
+ | | 7. Select //Update//. The program //Status// will specify that it is erasing flash. Once it has completed, the program //Status// will specify that it has completed. You can close the SAM Flasher Tool after this. | {{ : | ||
+ | | 8. To enter the application, | ||
---- | ---- | ||
{{navigation Advanced Audio Projects# | {{navigation Advanced Audio Projects# |