This is an old revision of the document!
Linux on the ADSP-SC5xx can be configured to boot from various sources (flash, network, SD Card, USB). For the Getting Started Guide we will configure the system so that the U-Boot bootloader is installed into flash on the development board. Linux and the filesystem will be downloaded at boot time via TFTP from your host PC, and copied into RAM. This method of network boot is convenient when developing Linux as it provides an easy method to update the image that is booted onto the board.
First you should make sure the U-boot has been written into the flash. You should see the outputs after powering up the board
U-Boot 2015.01 ADI-YOCTO-1.0.0 (May 14 2020 - 19:26:23) CPU: ADSP ADSP-SC589-0.1 (Detected Rev: 1.1) (spi flash boot) VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 450 MHz OCLK: 150 MHz Watchdog enabled I2C: ready DRAM: 224 MiB MMC: SC5XX SDH: 0 SF: Detected IS25LP512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB In: serial Out: serial Err: serial other init Net: dwmac.3100c000 Hit any key to stop autoboot: 0 sc #
If no output please refer this page Installing U-boot to build and write the U-Boot onto flash.
When you run printenv in u-Boot console, there will be 4 boot methods in the U-boot.
The default boot command is run ramboot.
Currently ADI provides some deploy methods to load linux kernel and boot into console. The default deploy method is ramboot.
In order to boot Linux, a copy of the image file should be copied into the /tftpboot directory. This file will be downloaded by U-Boot when the board begins to boot. In a console, in the build directory of your workspace issue the following commands:
$ cp build/tmp/deploy/images/<MACHINE>/zImage /tftpboot $ cp build/tmp/deploy/images/<MACHINE>/<DTB_FILE> /tftpboot $ cp build/tmp/deploy/images/<MACHINE>/<RAMDISK_FILE> /tftpboot/ramdisk.cpio.xz.u-boot
Where the macros in the above command are listed at the bottom of this page in Appendix.
Next, reboot the board and Linux will be downloaded to the target board and boot. When boot is successful you will be presented by the ADI logo and the login prompt:
sc # set serverip <SERVERIP> sc # set ipaddr <BOARD_IP> or sc # dhcp sc # sc # boot or sc # run ramboot ...... Starting syslogd/klogd: done * Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon ...done. @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ Analog Devices Yocto Distribution www.analog.com www.yoctoproject.org adsp-sc589-mini login: root Password: adi
The default username is root and the password is adi.
This boot method would finally use the Network File System which is stored in local Ubuntu Host. This is suggested when you do application development. For how to boot Linux via NFS, please refer to “How to Boot Linux From NFS”.
There are two kinds of boot commands for booting Linux from SD card.
ramboot_emmc
sdcardboot
And please make sure there are 500 MB at least in SD card to store zImge, dtb and system file.
For how to boot Linux via SD card, please refer to “How to Boot Linux From SD Card”
Due to the limited flash size, currently we can only support NOR boot the Linux kernel image(zImage) and device tree file(dtb). Put the filesystem in local HOST or SD Card is suggested.
MACHINE | DTB_FILE | RAMDISK_FILE |
---|---|---|
adsp-sc589-mini | sc589-mini.dtb | adsp-sc5xx-ramdisk-adsp-sc589-mini.cpio.xz.u-boot |
adsp-sc589-ezkit | sc589-ezkit.dtb | adsp-sc5xx-ramdisk-adsp-sc589-ezkit.cpio.xz.u-boot |
adsp-sc584-ezkit | sc584-ezkit.dtb | adsp-sc5xx-ramdisk-adsp-sc584-ezkit.cpio.xz.u-boot |
adsp-sc573-ezkit | sc573-ezkit.dtb | adsp-sc5xx-ramdisk-adsp-sc573-ezkit.cpio.xz.u-boot |
PREV: Building The Components HOME PAGE: Linux for ADSP-SC5xx Processors