Yocto requires the environment to be configured before building is possible. A setup-environment script in the griffin, gxp or gxp2 folder contains all the required environment settings.
$ source setup-environment -m adsp-sc589-ezkit
or
$ source setup-environment -m adsp-sc589-mini
or
$ source setup-environment -m adsp-sc594-som-ezkit
or
$ source setup-environment -m adsp-sc598-som-ezkit
Sourcing the script will configure your build environment and create a build folder along with a local build configuration file. See the Yocto Manual for further details.
The SDK can be built for the adsp-sc5xx-minimal image or the adsp-sc5xx-full image. To build the SDK for the adsp-sc5xx-minimal image invoke bitbake from within the build directory created previously.
$ bitbake adsp-sc5xx-minimal -c populate_sdk
or for the adsp-sc5xx-full image
$ bitbake adsp-sc5xx-full -c populate_sdk
When the build has completed you will find a set of files in the <BUILD_DIR>/tmp/deploy/sdk directory. For the minimal image on SC594:
$ ls tmp/deploy/sdk poky-glibc-x86_64-adsp-sc5xx-minimal-armv7at2hf-neon-adsp-sc594-som-ezkit-toolchain-3.1.8.host.manifest poky-glibc-x86_64-adsp-sc5xx-minimal-armv7at2hf-neon-adsp-sc594-som-ezkit-toolchain-3.1.8.sh poky-glibc-x86_64-adsp-sc5xx-minimal-armv7at2hf-neon-adsp-sc594-som-ezkit-toolchain-3.1.8.target.manifest poky-glibc-x86_64-adsp-sc5xx-minimal-armv7at2hf-neon-adsp-sc594-som-ezkit-toolchain-3.1.8.testdata.json
or the full image on SC598:
$ ls tmp/deploy/sdk poky-glibc-x86_64-adsp-sc5xx-full-aarch64-adsp-sc598-som-ezkit-toolchain-3.1.8.host.manifest poky-glibc-x86_64-adsp-sc5xx-full-aarch64-adsp-sc598-som-ezkit-toolchain-3.1.8.sh poky-glibc-x86_64-adsp-sc5xx-full-aarch64-adsp-sc598-som-ezkit-toolchain-3.1.8.target.manifest poky-glibc-x86_64-adsp-sc5xx-full-aarch64-adsp-sc598-som-ezkit-toolchain-3.1.8.testdata.json
The poky-glibc-x86_64-adsp-sc5xx-minimal-armv7at2hf-neon-adsp-sc594-som-ezkit-toolchain-3.1.8.sh and the poky-glibc-x86_64-adsp-sc5xx-full-aarch64-adsp-sc598-som-ezkit-toolchain-3.1.8.sh are self-extracting archives containing the SDK.
Invoke the self-extracting archive. It will default to installing to /opt/poky/3.1.8 but gives you the option to select your own install folder during the installation. For the minimal image on SC594
$ ./poky-glibc-x86_64-adsp-sc5xx-minimal-armv7at2hf-neon-adsp-sc594-som-ezkit-toolchain-3.1.8.sh Poky (Yocto Project Reference Distro) SDK installer version 3.1.8 ================================================================= Enter target directory for SDK (default: /opt/poky/3.1.8): You are about to install the SDK to "/opt/poky/3.1.8". Proceed [Y/n]? y Extracting SDK...................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /opt/poky/3.1.8/environment-setup-armv7at2hf-neon-poky-linux-gnueabi
or for the full image on SC598
./tmp/deploy/sdk/poky-glibc-x86_64-adsp-sc5xx-full-aarch64-adsp-sc598-som-ezkit-toolchain-3.1.8.sh Poky (Yocto Project Reference Distro) SDK installer version 3.1.8 ================================================================= Enter target directory for SDK (default: /opt/poky/3.1.8): You are about to install the SDK to "/opt/poky/3.1.8". Proceed [Y/n]? y Extracting SDK................................................................................................................................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /opt/poky/3.1.8/environment-setup-aarch64-poky-linux
Your SDK is now installed.