The build system is currently supported on host PCs running Ubuntu 20.04 LTS 64-bit.
In order to build and deploy Linux to your ADSP-SC589-EZKIT or ADSP-SC589-MINI development board you will need to install the following packages on your host PC.
$ sudo apt-get update $ sudo apt-get install -y gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev xterm u-boot-tools openssl curl tftpd-hpa python
CrossCore Embedded Studio contains OpenOCD which is used to transfer U-Boot into RAM for the first initial boot of the device. The tools are created for 32-bit architecture and therefore requires a 32-bit libz package to run. Download and install it.
$ wget http://download.analog.com/tools/CrossCoreEmbeddedStudio/Releases/Release_2.10.0/adi-CrossCoreEmbeddedStudio-linux-x86-2.10.0.deb $ sudo dpkg -i ./adi-CrossCoreEmbeddedStudio-linux-x86-2.10.0.deb $ sudo apt install lib32z1
A TFTP server on the host is used to transfer images to the development board. Install and configure.
$ sudo vi /etc/default/tftpd-hpa #Replace the existing file with the following TFTP_USERNAME="tftp" TFTP_DIRECTORY="/tftpboot" TFTP_ADDRESS="0.0.0.0:69" TFTP_OPTIONS="--secure" #End of File $ sudo mkdir /tftpboot $ sudo chmod 777 /tftpboot $ sudo service tftpd-hpa restart
In order to communicate with the U-Boot bootloader, a UART connection must be made between the host PC and the development board. It is recommended that you use minicom to do this. Minicom must be configured to connect to U-Boot correctly.
On the host PC open a terminal and execute the following commands:
$ sudo apt-get install -y minicom $ sudo minicom -s +-----[configuration]------+ | Filenames and paths | | File transfer protocols | | Serial port setup | | Modem and dialing | | Screen and keyboard | | Save setup as dfl | | Save setup as.. | | Exit | | Exit from Minicom | +--------------------------+ # Select Serial port setup Set Serial Device to /dev/ttyUSB0 Set Bps/Par/Bits to 115200 8N1 Set Hardware Flow Control to No Close the Serial port setup option by press Esc Select Save setup as dfl Select Exit
The example is fully contained in the Analog Devices Yocto Linux github repositories.
To install the sources:
$ mkdir ~/griffin $ cd ~/griffin $ mkdir bin $ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ./bin/repo $ chmod a+x ./bin/repo $ ./bin/repo init \ -u https://github.com/analogdevicesinc/lnxdsp-repo-manifest.git \ -b release/yocto-2.1.0 \ -m release-yocto-2.1.0.xml $ ./bin/repo sync
Yocto requires the environment to be configured before building is possible. A setup-environment script in the griffin folder contains all the required environment settings for your build target. Source the setup script for your board:
$ source setup-environment -m adsp-sc589-ezkit
or
$ source setup-environment -m adsp-sc589-mini
Sourcing the script will configure your build environment and create a build folder along with a local build configuration file. See the Yocto Manual for further details.
You can build three different versions of the root file system; minimal, ramdisk and full. To build the example images invoke bitbake from within the build directory created previously.
$ bitbake adsp-sc5xx-minimal $ bitbake adsp-sc5xx-ramdisk $ bitbake adsp-sc5xx-full
When the build completes you will see a warning that the ELF binary has relocations in .text. It is OK to ignore this warning
Copy the U-Boot binary files to the tftp directory:
$ cp tmp/deploy/images/adsp-sc589-ezkit/init-sc589-ezkit.elf /tftpboot $ cp tmp/deploy/images/adsp-sc589-ezkit/u-boot-sc589-ezkit /tftpboot $ cp tmp/deploy/images/adsp-sc589-ezkit/u-boot-sc589-ezkit.ldr /tftpboot
or
$ cp tmp/deploy/images/adsp-sc589-mini/init-sc589-mini.elf /tftpboot $ cp tmp/deploy/images/adsp-sc589-mini/u-boot-sc589-mini /tftpboot $ cp tmp/deploy/images/adsp-sc589-mini/u-boot-sc589-mini.ldr /tftpboot
Before installing the software on to the development board, ensure that the following cables are connected:
The console output from U-Boot and later on Linux will appear on the USB serial port configured in minicom earlier so open up minicom.
Terminal1: minicom
$ sudo minicom
In a separate console launch OpenOCD and connect to the development board
Terminal2: OpenOCD
$ cd /opt/analog/cces/2.10.0/ARM/openocd/share/openocd/scripts $ sudo /opt/analog/cces/2.10.0/ARM/openocd/bin/openocd -f interface/<ICE>.cfg -f board/adspsc589_ezbrd.cfg
Where <ICE> should be replaced with ice1000 or ice2000 depending on your hardware. When successful you should see a message similar to the console output below
Open On-Chip Debugger (Analog Devices CCES 2.10.0 OpenOCD 0.9.0-ga8d0a22) 0.9.0 Licensed under GNU GPL v2 Report bugs to <processor.tools.support@analog.com> adapter speed: 1000 kHz Info : transports supported by the debug adapter: "jtag", "swd" Info : auto-select transport "jtag" halt and restart using CTI trst_only separate trst_push_pull Info : ICE-1000 firmware version is 1.0.2 Info : clock speed 1000 kHz Info : JTAG tap: adspsc58x.adjc tap/device found: 0x228080cb (mfg: 0x065, part: 0x2808, ver: 0x2) Info : JTAG tap: adspsc58x.dap enabled Info : adspsc58x.dap: hardware has 3 breakpoints, 2 watchpoints Info : adspsc58x.dap: but you can only set 1 watchpoint
In a third console window launch GDB and type target extended-remote :3333
. This will make GDB to connect to the gdbserver on the local host using port 3333. Then, load the init file into RAM by typing load init-sc589-ezkit.elf
or load init-sc589-mini.elf
and run it by typing c
. Hit Ctrl+C to interrupt thereafter.
Terminal3: GDB (sc589-ezkit)
$ cd /tftpboot $ /opt/analog/cces/2.10.0/ARM/arm-none-eabi/bin/arm-none-eabi-gdb u-boot-sc589-ezkit ... (gdb) target extended-remote :3333 Remote debugging using :3333 0x00004884 in ?? () (gdb) load init-sc589-ezkit.elf Loading section .text, size 0xa70 lma 0x20080000 Start address 0x20080028, load size 2672 Transfer rate: 25 KB/sec, 2672 bytes/write. (gdb) c Continuing. ^C Program received signal SIGINT, Interrupt. 0x20080024 in ?? ()
Terminal3: GDB (sc589-mini)
$ cd /tftpboot $ /opt/analog/cces/2.10.0/ARM/arm-none-eabi/bin/arm-none-eabi-gdb u-boot-sc589-ezkit ... (gdb) target remote :3333 Remote debugging using :3333 0x00004884 in ?? () (gdb) load init-sc589-mini.elf Loading section .text, size 0xa70 lma 0x20080000 Start address 0x20080028, load size 2672 Transfer rate: 25 KB/sec, 2672 bytes/write. (gdb) c Continuing. ^C Program received signal SIGINT, Interrupt. 0x20080024 in ?? ()
Now, load U-Boot into RAM.
Terminal3: GDB (sc589-ezkit)
(gdb) load Loading section .text, size 0x3a8 lma 0x89200000 Loading section .efi_runtime, size 0xe30 lma 0x892003a8 Loading section .text_rest, size 0x4dd10 lma 0x892011e0 Loading section .rodata, size 0xfbe0 lma 0x8924eef0 Loading section .hash, size 0x18 lma 0x8925ead0 Loading section .dtb.init.rodata, size 0x360 lma 0x8925eaf0 Loading section .data, size 0x3468 lma 0x8925ee50 Loading section .got.plt, size 0xc lma 0x892622b8 Loading section .u_boot_list, size 0xe80 lma 0x892622c4 Loading section .efi_runtime_rel, size 0xd0 lma 0x89263144 Loading section .rel.dyn, size 0xb180 lma 0x89263214 Loading section .dynsym, size 0x30 lma 0x8926e394 Loading section .dynstr, size 0x1 lma 0x8926e3c4 Loading section .dynamic, size 0x90 lma 0x8926e3c8 Loading section .gnu.hash, size 0x18 lma 0x8926e458 Start address 0x89200000, load size 451677 Transfer rate: 31 KB/sec, 11581 bytes/write. (gdb) c Continuing.
Terminal3: GDB (sc589-mini)
(gdb) load Loading section .text, size 0x3a8 lma 0xc2200000 Loading section .efi_runtime, size 0xe30 lma 0xc22003a8 Loading section .text_rest, size 0x4f4a0 lma 0xc22011e0 Loading section .rodata, size 0xff43 lma 0xc2250680 Loading section .hash, size 0x18 lma 0xc22605c4 Loading section .dtb.init.rodata, size 0x360 lma 0xc22605e0 Loading section .data, size 0x3390 lma 0xc2260940 Loading section .got.plt, size 0xc lma 0xc2263cd0 Loading section .u_boot_list, size 0xe80 lma 0xc2263cdc Loading section .efi_runtime_rel, size 0xd0 lma 0xc2264b5c Loading section .rel.dyn, size 0xb218 lma 0xc2264c2c Loading section .dynsym, size 0x30 lma 0xc226fe44 Loading section .dynstr, size 0x1 lma 0xc226fe74 Loading section .dynamic, size 0x90 lma 0xc226fe78 Loading section .gnu.hash, size 0x18 lma 0xc226ff08 Start address 0xc2200000, load size 458512 Transfer rate: 30 KB/sec, 11462 bytes/write. (gdb) c Continuing.
At this point U-Boot will now be running in RAM on your target board. You should see U-Boot booting in the minicom console (Terminal 1). Press a key to interrupt the boot process before the countdown terminates:
Terminal1: minicom (sc589-ezkit)
U-Boot 2020.10 (Aug 23 2022 - 13:09:23 +0000) CPU: ADSP ADSP-SC589-0.1 (Detected Rev: 1.1) (spi flash boot) VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 450 MHz OCLK: 150 MHz Model: ADI sc589-ezkit I2C: ready DRAM: 224 MiB MMC: SC5XX SDH: 0 Loading Environment from SPIFlash... SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB *** Warning - bad CRC, using default environment In: serial@0x31003000 Out: serial@0x31003000 Err: serial@0x31003000 SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB other init Net: dwmac.3100c000 Hit any key to stop autoboot: 0 =>
Terminal1: minicom (sc589-mini)
U-Boot 2020.10 (Aug 23 2022 - 13:09:23 +0000) CPU: ADSP ADSP-SC589-0.1 (Detected Rev: 1.1) (spi flash boot) VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 450 MHz OCLK: 150 MHz Model: ADI sc589-mini I2C: ready DRAM: 224 MiB MMC: SC5XX SDH: 0 Loading Environment from SPIFlash... SF: Detected is25lp512 with page size 256 Bytes, erase size 64 KiB, total 64 MiB *** Warning - bad CRC, using default environment In: serial@0x31003000 Out: serial@0x31003000 Err: serial@0x31003000 other init Net: dwmac.3100c000 Hit any key to stop autoboot: 0 =>
In the U-Boot console, set the IP address of the Host Linux PC that hosts the U-Boot loader file (u-boot-sc573-ezkit.ldr
) on TFTP.
Terminal1: minicom
=> setenv serverip <SERVERIP>
ip addr
command from the shell or console.
If your network supports DHCP, run:
=> dhcp
If your network does NOT support DHCP, run:
=> set ipaddr <ADDR>
Where <ADDR>
is the IP address you want to assign.
Next, run the U-Boot update command to copy the U-Boot loader file from the host PC to the target board, and write it into flash:
=> run update
You will see an output similar to the one below:
=> run update Speed: 1000, full duplex Using dwmac.3100c000 device TFTP from server 192.168.1.223; our IP address is 192.168.1.218 Filename 'u-boot-sc589-ezkit.ldr'. Load address: 0xc2000000 Loading: ################################ 3.8 MiB/s done Bytes transferred = 459144 (70188 hex) SF: Detected w25q128 with page size 256 Bytes, erase size 4 KiB, total 16 MiB SF: 524288 bytes @ 0x0 Erased: OK device 0 offset 0x0, size 0x70188 SF: 459144 bytes @ 0x0 Written: OK =>
At this point the U-Boot binary is stored in flash. You can now disconnect the ICE-1000 or ICE-2000 from the development board and make sure to switch the BMODE to position 1. You will only need to reconnect this if your board fails to boot and you need to re-follow these instructions.
In order to use an SD Card with Linux we need to prepare it by formatting it in the correct format. This section of instructions requires you to correctly identify the SD Card and format the card. If you select the wrong drive you may cause irreversible damage to you Host PC. To format the SD Card, follow the commands below. The example code in this section assumes that the SD Card device is reported to be /dev/sdb. Ensure that you change these commands to use your device.
$ sudo fdisk /dev/sdb /* Create primary partition 1, 256M size*/ Command (m for help): n Select (default p): p Partition number (1-4, default 1): 1 First sector (2048-3887103, default 2048): PRESS ENTER Last sector, +sectors or +size{K,M,G} (2048-3887103, default 3887103): PRESS ENTER /* Save partition */ Command (m for help): w
Format the SD card to EXT filesystem
$ sudo mkfs.ext2 /dev/sdb1
Next, we need to copy the Linux file system and kernel image to the SD Card. We install this on to the SD Card by mounting the file system on to the local Host PC and copying the contents on to the SD Card. To allow the choice of booting using ramboot and sdcard boot we copy the ramboot image to the SD card as well as extract the minimal image to the SD card.
$ mkdir ~/mnt $ sudo mount -t ext2 /dev/sdb1 ~/mnt $ sudo mkdir ~/mnt/boot $ sudo cp tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-ramdisk-adsp-sc589-ezkit.cpio.xz.u-boot ~/mnt/boot/ramdisk.cpio.xz.u-boot $ sudo cp tmp/deploy/images/adsp-sc589-ezkit/sc589-ezkit.dtb ~/mnt/boot/ $ sudo cp tmp/deploy/images/adsp-sc589-ezkit/fitImage ~/mnt/boot/ $ sudo tar -xf tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-minimal-adsp-sc589-ezkit.tar.xz -C ~/mnt $ sudo umount ~/mnt
or
$ mkdir ~/mnt $ sudo mount -t ext2 /dev/sdb1 ~/mnt $ sudo mkdir ~/mnt/boot $ sudo cp tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-ramdisk-adsp-sc589-mini.cpio.xz.u-boot ~/mnt/boot/ramdisk.cpio.xz.u-boot $ sudo cp tmp/deploy/images/adsp-sc589-mini/sc589-mini.dtb ~/mnt/boot/ $ sudo cp tmp/deploy/images/adsp-sc589-mini/fitImage ~/mnt/boot/ $ sudo tar -xf tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-minimal-adsp-sc589-mini.tar.xz -C ~/mnt $ sudo umount ~/mnt
The file system and kernel image are now installed on to the SD Card. The SD Card can now be safely removed from the Host PC.
Insert the SD card to target board, and reset the board and enter into U-Boot
=> run sdcardboot or => run ramboot_emmc
The linux kernel will then boot up using the file system stored in SD card.
In order to boot Linux, the TFTP server should be setup as above and (for both NFS and RAM boot) a copy of the kernel image should be copied into the /tftpboot directory.
$ cp tmp/deploy/images/adsp-sc589-ezkit/fitImage /tftpboot
or
$ cp tmp/deploy/images/adsp-sc589-mini/fitImage /tftpboot
For RAM boot we need to copy the image containing filesystem to the /tftpboot directory.
$ cp tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-ramdisk-adsp-sc589-ezkit.cpio.xz.u-boot /tftpboot/ramdisk.cpio.xz.u-boot
or
$ cp tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-ramdisk-adsp-sc589-mini.cpio.xz.u-boot /tftpboot/ramdisk.cpio.xz.u-boot
For NFS boot we use the Network File System which is stored in local Ubuntu Host. This is suggested when you do application development. To setup the NFS server:
$ sudo apt-get install nfs-kernel-server $ sudo vi /etc/exports #Add following commands /romfs *(rw,sync,no_root_squash,no_subtree_check) $ sudo mkdir /romfs/ $ sudo chmod 777 /romfs/ $ sudo service nfs-kernel-server start
The output will indicate that the server is active, i.e.
● nfs-server.service - NFS server and services Loaded: loaded (/lib/systemd/system/nfs-server.service; enabled; vendor preset: enabled) Drop-In: /run/systemd/generator/nfs-server.service.d └─order-with-mounts.conf Active: active (exited) since Tue 2022-09-06 14:38:31 BST; 3 months 14 days ago Main PID: 953 (code=exited, status=0/SUCCESS) Tasks: 0 (limit: 18797) Memory: 0B CGroup: /system.slice/nfs-server.service Sep 06 14:38:29 $YOUR_HOSTNAME systemd[1]: Starting NFS server and services... Sep 06 14:38:31 $YOUR_HOSTNAME systemd[1]: Finished NFS server and services.
If it's reported as inactive, wait a few moments and check the status again.
The file system is then copied to /romfs.
If you are using the ADSP-SC589-EZKIT with the full image (you ran 'bitbake adsp-sc5xx-full'):
$ sudo tar -xf tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-full-adsp-sc589-ezkit.tar.xz -C /romfs
Or if you are using the ADSP-SC589-EZKIT with the minimal image (you ran 'bitbake adsp-sc5xx-minimal'):
$ sudo tar -xf tmp/deploy/images/adsp-sc589-ezkit/adsp-sc5xx-minimal-adsp-sc589-ezkit.tar.xz -C /romfs
Or if you are using the ADSP-SC589-MINI with the full image (you ran 'bitbake adsp-sc5xx-full'):
$ sudo tar -xf tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-full-adsp-sc589-mini.tar.xz -C /romfs
Or if you are using the ADSP-SC589-MINI with the minimal image (you ran 'bitbake adsp-sc5xx-minimal'):
$ sudo tar -xf tmp/deploy/images/adsp-sc589-mini/adsp-sc5xx-minimal-adsp-sc589-mini.tar.xz -C /romfs
Next, on the target, from u-boot, run one of the following command:
=> run ramboot or => run nfsboot ...... ...... Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@ @@@@@@@@ @@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@ @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@ Analog Devices Yocto Distribution www.analog.com www.yoctoproject.org adsp-sc589-ezkit login: root Password: adi root@adsp-sc589-ezkit:~#
The default username is root and the password is adi.
To build the SDK follow the instructions here Building the SDK.