This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:device_mode:gdaget_eth [15 Jul 2020 11:30] cathy fang [Example Usage] |
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:usb:device_mode:gdaget_eth [27 Jan 2021 22:35] Robin Getz use wp> interwiki links |
||
---|---|---|---|
Line 1: | Line 1: | ||
====== USB Gadget Ethernet ====== | ====== USB Gadget Ethernet ====== | ||
- | Gadget Ethernet allows [[https://en.wikipedia.org/wiki/Ethernet_over_USB|Ethernet emulation over USB]], allowing the reading/writing at higher speeds than most Wifi connections. This page provides a approach how to use the USB Gadget Ethernet Feature on ADSP-SC5XX board and give a brief Example usage: | + | Gadget Ethernet allows [[wp>Ethernet_over_USB|Ethernet emulation over USB]], allowing the reading/writing at higher speeds than most Wifi connections. This page provides a approach how to use the USB Gadget Ethernet Feature on ADSP-SC5xx board and give a brief Example usage: |
---- | ---- | ||
Line 42: | Line 42: | ||
[*] RNDIS support | [*] RNDIS support | ||
</code> | </code> | ||
- | <WRAP center round todo 100%> | + | |
- | ifconfig and some commands depend on the ethnert feature | + | |
- | </WRAP> | + | |
---- | ---- |