SC5xx processors feature an up/down counter and thumbwheel interface.
A 32-bit up/down counter is provided that can sense 2-bit quadrature or binary codes as typically emitted by industrial drives or manual thumb wheels. The counter can also operate in general-purpose up/down count modes, in which case count direction is either controlled by a level sensitive input pin or by two edge detectors. A third input can provide flexible zero marker support and can alternatively be used to input the push-button signal of thumb wheels. All three pins have a programmable debouncing circuit.
An ADSP-SC5xx EZ-Board:
The SC589-EZKIT board does not include the rotary input hardware.
You need to enable the ADI rotary driver in Linux kernel.
Device Drivers ---> Input device support ---> <*> Event interface [*] Miscellaneous devices ---> <*> ADI Rotary support
You should also enable the event test program to assist with testing. Add the event test program in the filesystem images, it's enabled in adsp-sc5xx-full image by default.
vim build/conf/local.conf IMAGE_INSTALL_append = "evtest"
As the Rotary hardware pin conflicts with MSI function on the ADSP-SC573 EZ-Board, thumb wheel switch is disabled by default in U-Boot for ADSP-SC573 EZ-Board out of box. To enable thumb wheel hardware switch, you should enable the thumb wheel switch in U-Boot and disable MSI function in Linux kernel. Please refer to ADSP-SC573 EZ-Board schematic and the section Mobile Storage Interface for MMC/SD for more information.
Device Drivers MMC/SD/SDIO card support ---> [*] Synopsys DesignWare Memory Card Interface [*] Synopsys Designware MCI Support as platform device <N> ADI specific extensions for Synopsys DW Memory Card Interface
As the Rotary hardware pin conflicts with EMAC RESET pin of Ethernet PHY DP83865/BCM89810 on the ADSP-SC584 EZ-Board, you should disable Ethernet function in Linux kernel. Please refer to ADSP-SC584 EZ-Board schematic and the section Ethernet driver and performance for more information.
Device Drivers ---> [*] Network device support ---> [*] Ethernet driver support ---> [*] STMicroelectronics devices <N> STMicroelectronics 10/100/1000 Ethernet driver <N> STMMAC Platform bus support
Device Drivers ---> [*] Network device support ---> -*- PHY Device support and infrastructure ---> <N> National Semiconductor PHYs
The driver provides two options. It can either send Key (KEY) or Relative (REL) events.
Option 1 – send Key events: Provide two KEY Codes for:
rotary_up_key = KEY_PLUS rotary_down_key = KEY_MINUS
Option 2 – send REL events: Provide one REL event type:
rotary_rel_code = REL_WHEEL
In case your CZM input is connected (push-button signal of thumb wheels) Specify the KEY event – this will enable the CZM input. See include/linux/input.h for a full list of supported events.
rotary_button_key = KEY_ENTER
The debounce prescale value is used to select the noise filtering characteristic of the input pins. Must be in the range of 0..17
debounce = 10
The driver supports various Counter types
cnt_mode = CNTMODE_QUADENC
You will get following information when the rotary hardware device is turned left, right or pushed.
# evtest /dev/input/event0 Input driver version is 1.0.1 Input device ID: bus 0x19 vendor 0x1 product 0x1 version 0x100 Input device name: "3100b000.cnt" Supported events: Event type 0 (Sync) Event type 1 (Key) Event code 28 (Enter) Event type 3 (Absolute) Event code 8 (Wheel) Value 0 Min -256 Max 256 Testing ... (interrupt to exit) Event: time 172.195518, type 3 (Absolute), code 8 (Wheel), value 1 Event: time 172.195518, -------------- Report Sync ------------ Event: time 172.206199, type 3 (Absolute), code 8 (Wheel), value 2 Event: time 172.206199, -------------- Report Sync ------------ Event: time 172.211954, type 3 (Absolute), code 8 (Wheel), value 3 Event: time 172.211954, -------------- Report Sync ------------ Event: time 172.218301, type 3 (Absolute), code 8 (Wheel), value 4 Event: time 172.218301, -------------- Report Sync ------------ Event: time 172.401334, type 3 (Absolute), code 8 (Wheel), value 5 Event: time 172.401334, -------------- Report Sync ------------ Event: time 172.485123, type 3 (Absolute), code 8 (Wheel), value 4 Event: time 172.485123, -------------- Report Sync ------------ Event: time 173.511092, type 3 (Absolute), code 8 (Wheel), value 3 Event: time 173.511092, -------------- Report Sync ------------ Event: time 173.565120, type 3 (Absolute), code 8 (Wheel), value 2 Event: time 173.565120, -------------- Report Sync ------------ Event: time 173.582020, type 3 (Absolute), code 8 (Wheel), value 1 Event: time 173.582020, -------------- Report Sync ------------ Event: time 173.600967, type 3 (Absolute), code 8 (Wheel), value 0 Event: time 173.600967, -------------- Report Sync ------------ Event: time 175.609542, type 3 (Absolute), code 8 (Wheel), value 1 Event: time 175.609542, -------------- Report Sync ------------ Event: time 175.624487, type 3 (Absolute), code 8 (Wheel), value 2 Event: time 175.624487, -------------- Report Sync ------------ Event: time 175.629124, type 3 (Absolute), code 8 (Wheel), value 3 Event: time 175.629124, -------------- Report Sync ------------ Event: time 175.633278, type 3 (Absolute), code 8 (Wheel), value 4 Event: time 175.633278, -------------- Report Sync ------------ Event: time 176.719340, type 3 (Absolute), code 8 (Wheel), value 5 Event: time 176.719340, -------------- Report Sync ------------ Event: time 176.741497, type 3 (Absolute), code 8 (Wheel), value 6 Event: time 176.741497, -------------- Report Sync ------------ Event: time 176.748370, type 3 (Absolute), code 8 (Wheel), value 7 Event: time 176.748370, -------------- Report Sync ------------ Event: time 176.754401, type 3 (Absolute), code 8 (Wheel), value 8 Event: time 176.754401, -------------- Report Sync ------------ Event: time 177.670738, type 3 (Absolute), code 8 (Wheel), value 9 Event: time 177.670738, -------------- Report Sync ------------ Event: time 177.691486, type 3 (Absolute), code 8 (Wheel), value 10 Event: time 177.691486, -------------- Report Sync ------------ Event: time 177.698444, type 3 (Absolute), code 8 (Wheel), value 11 Event: time 177.698444, -------------- Report Sync ------------ Event: time 177.705056, type 3 (Absolute), code 8 (Wheel), value 12 Event: time 177.705056, -------------- Report Sync ------------ Event: time 178.598188, type 3 (Absolute), code 8 (Wheel), value 11 Event: time 178.598188, -------------- Report Sync ------------ Event: time 178.700345, type 3 (Absolute), code 8 (Wheel), value 10 Event: time 178.700345, -------------- Report Sync ------------ Event: time 178.710039, type 3 (Absolute), code 8 (Wheel), value 9 Event: time 178.710039, -------------- Report Sync ------------ Event: time 178.716659, type 3 (Absolute), code 8 (Wheel), value 8 Event: time 178.716659, -------------- Report Sync ------------ Event: time 179.628879, type 3 (Absolute), code 8 (Wheel), value 7 Event: time 179.628879, -------------- Report Sync ------------ Event: time 179.705605, type 3 (Absolute), code 8 (Wheel), value 6 Event: time 179.705605, -------------- Report Sync ------------ Event: time 179.714243, type 3 (Absolute), code 8 (Wheel), value 5 Event: time 179.714243, -------------- Report Sync ------------ Event: time 179.719841, type 3 (Absolute), code 8 (Wheel), value 4 Event: time 179.719841, -------------- Report Sync ------------
Back to Kernel Features and Device Drivers for ADSP-SC5xx Yocto Linux