This is an old revision of the document!
The Yocto Linux Product provides user space APIs that allow applications to easily communicate with the SHARC cores of the ADSP-SC5xx processor.
Communication is performed using the Multi-core Communications API (MCAPI) specification which defines an API and a semantics for communication and synchronization between processing cores in embedded systems. MCAPI is supported on the SHARC cores of the ADSP-SC5xx processors in both bare-metal and RTOS using CrossCore Embedded Studio. For more information about MCAPI, please refer to the MCAPI Specification document from MCAPI.org.
ADSP-SC5xx is a series of products with multiple processor cores (two SHARC+ cores and an ARM® Cortex-A5 processor), this page provides some approaches to support the multi-core communication/control termed as the Internal Cores Communications (ICC) which contains the sections:
Core Control
RemoteProc
:[[resources:tools-software/linuxdsp/docs/linux-kernel-and-drivers/mcapi/sec_driver_and_multicore_development|SEC driver and multicore development]]
MCAPI
Back to Kernel Features and Device Drivers for ADSP-SC5xx Yocto Linux