This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:mcapi_example [24 Jul 2020 11:13] – [Step6: Run Linux MCAPI MSG Demo Test] Sunny Feng | resources:tools-software:linuxdsp:docs:linux-kernel-and-drivers:mcapi:mcapi_example [26 Jul 2020 05:29] – [Get the Source Code Ready] Sunny Feng | ||
---|---|---|---|
Line 17: | Line 17: | ||
The MCAPI example for ARM core (Running Linux) is included in the YOCTO, and you can get the MCAPI example for SHARC+ Cores from the gitbub [[https:// | The MCAPI example for ARM core (Running Linux) is included in the YOCTO, and you can get the MCAPI example for SHARC+ Cores from the gitbub [[https:// | ||
- | **MCAPI Examples for SHARC Cores ** | + | ===MCAPI Examples for SHARC Cores=== |
- | ; | + | ; name : lnxdsp-exmaples/ |
- | ; **name** : lnxdsp-exmaples/ | + | ; version : '' |
- | ; **version** : '' | + | ; branch : remotes/ |
- | ; **branch** : remotes/ | + | |
**__Git Usage__** | **__Git Usage__** | ||
Line 32: | Line 31: | ||
</ | </ | ||
- | **MCAPI Examples for ARM Core** | + | ===MCAPI Examples for ARM Core=== |
* sources/ | * sources/ | ||
* sources/ | * sources/ | ||
- | **CCES** | + | ===CCES=== |
* Analog Devices [[https:// | * Analog Devices [[https:// |