This is an old revision of the document!
This document talks about how we can load files on USB memory stick, into system RAM from u-boot. Here we take ADSP-SC573 board as example.
Connect USB stick to the USB OTG port, via the USB adapter cable, as following, and reset the board
Insert the USB memory stick into a Linux PC, you will see new items show up in /dev/sd*, as following:
$ ls /dev/sd* /dev/sda /dev/sda1 /dev/sda2 /dev/sda5 /dev/sdb /dev/sdb1
In this case the /dev/sdb is for the USB stick we just plugged in.
Caution : Please double check the device node newly created for your memory stick, otherwise serious damage like system permanent crash down happens!
The format a vfat partiton on it:
$ sudo mkfs.vfat /dev/sdb1 [sudo] password for ... mkfs.vfat 3.0.12 (29 Oct 2011)
$ sudo mount /dev/sdb1 /mnt $ sudo cp build/tmp/deploy/images/<MACHINE>/<RAMDISK_FILE> /mnt/boot/ramdisk.cpio.xz.u-boot $ sudo cp build/tmp/deploy/images/<MACHINE>/<DTB_FILE> /mnt/boot/ $ sudo cp build/tmp/deploy/images/<MACHINE>/zImage /mnt/boot/ $ sudo umount /mnt
Then plug the USB stick to the USB OTG port in board, via the USB adapter cable, and reset the board
Run “start usb” In the u-boot console:
sc # usb start (Re)start USB... USB0: scanning bus 0 for devices... 1 USB Device(s) found scanning usb for storage devices... 1 Storage Device(s) found
Run “fatls usb 0:1” In the u-boot console:
sc # fatls usb 0:1 4231792 zImage 21512 sc589-ezkit.dtb 12225998 ramdisk.cpio.xz.u-boot 3 file(s), 0 dir(s)
This shows the FAT files information in USB device 0 partition 1, with files we copied.
As example we load both the dtb, zImage and the ramdisk file into proper location.
Don't forget to change the file/dtb name and load address according to your board type (i.e. SC589-ezkit or SC584-ezkit or SC573-ezkit), otherwise it may not boot properly.
sc # fatload usb 0:1 ${dtbaddr} ${dtbfile} reading sc589-ezkit.dtb 19120 bytes read in 30 ms (335 KiB/s) sc # fatload usb 0:1 ${loadaddr} ${ramfile} reading zImage 4106096 bytes read in 2610 ms (1.5 MiB/s) sc # fatload usb 0:1 ${initramaddr} ${initramfile} reading ramdisk.cpio.xz.u-boot 12225833 bytes read in 7772 ms (1.5 MiB/s)
Verify the read operation:
sc # bootz ${loadaddr} ${initramaddr} ${dtbaddr} Kernel image @ 0xc2000000 [ 0x000000 - 0x3ea770 ] ## Loading init Ramdisk from Legacy Image at c5000000 ... Image Name: Analog Devices Ram Disk Image Image Type: ARM Linux RAMDisk Image (gzip compressed) Data Size: 12225769 Bytes = 11.7 MiB Load Address: 00000000 Entry Point: 00000000 Verifying Checksum ... OK ## Flattened Device Tree blob at c4000000 Booting using the fdt blob at 0xc4000000 Loading Ramdisk to cf2b7000, end cfe5fce9 ... OK Loading Device Tree to cf2af000, end cf2b6aaf ... OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Booting Linux on physical CPU 0x0 Linux version 4.19.0-yocto-standard (oe-user@oe-host) (gcc version 8.2.0 (GCC)) #1 Fri Jul 31 10:34:04 UTC 2020 CPU: ARMv7 Processor [410fc051] revision 1 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache OF: fdt: Machine model: ADI sc589-mini bootconsole [earlycon0] enabled Memory policy: Data cache writeback Hit pending asynchronous external abort (FSR=0x00001c06) during first unmask, this is most likely caused by a firmware/bootloader bug. CPU: All CPU(s) started in SVC mode. dump init clock rate CGU0_PLL 450 MHz CGU0_SYSCLK 225 MHz CGU0_CCLK 450 MHz CGU0_SYS0 112 MHz CGU0_DCLK 450 MHz CGU0_OCLK 150 MHz CGU0_SYS0 112 MHz random: get_random_bytes called from start_kernel+0x98/0x3dc with crng_init=0 Built 1 zonelists, mobility grouping on. Total pages: 56896 Kernel command line: root=/dev/mtdblock2 rw rootfstype=jffs2 clkin_hz=(25000000) earlyprintk=serial,uart0,57600 console=ttySC0,57600 mem=224M ip=10.99.24.96:10.99.24.65:10.99.24.1:255.255.255.0:sc58x:ethf Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) Memory: 205764K/229376K available (6144K kernel code, 200K rwdata, 1512K rodata, 1024K init, 112K bss, 23612K reserved, 0K cma-reserved) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xffc00000 - 0xfff00000 (3072 kB) vmalloc : 0xce800000 - 0xff800000 ( 784 MB) lowmem : 0xc0000000 - 0xce000000 ( 224 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .text : 0x(ptrval) - 0x(ptrval) (7136 kB) .init : 0x(ptrval) - 0x(ptrval) (1024 kB) .data : 0x(ptrval) - 0x(ptrval) ( 201 kB) .bss : 0x(ptrval) - 0x(ptrval) ( 113 kB) NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 clocksource: cs_gptimer: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 16988981748 ns sched_clock: 32 bits at 112MHz, resolution 8ns, wraps every 19088743419ns Console: colour dummy device 80x30 Calibrating delay loop... 297.98 BogoMIPS (lpj=595968) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) CPU: Testing write buffer coherency: ok Setting up static identity map for 0xc2100000 - 0xc210003c devtmpfs: initialized VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns futex hash table entries: 256 (order: -1, 3072 bytes) pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations L2C: device tree omits to specify unified cache L2C-310 dynamic clock gating enabled, standby mode enabled L2C-310 cache controller enabled, 8 ways, 256 kB L2C-310: CACHE_ID 0x410000c9, AUX_CTRL 0x06040000 sc58x_init: registering device resources sec init... enabled hw-breakpoint: Failed to enable monitor mode on CPU 0. ADI DMA2 Controller SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb i2c-adi-twi 31001400.twi: ADI on-chip I2C TWI Controller, regs_base@(ptrval) i2c-adi-twi 31001500.twi: ADI on-chip I2C TWI Controller, regs_base@(ptrval) i2c-adi-twi 31001600.twi: ADI on-chip I2C TWI Controller, regs_base@(ptrval) pps_core: LinuxPPS API ver. 1 registered pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> PTP clock support registered Advanced Linux Sound Architecture Driver Initialized. clocksource: Switched to clocksource cs_gptimer NET: Registered protocol family 2 tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) TCP established hash table entries: 2048 (order: 1, 8192 bytes) TCP bind hash table entries: 2048 (order: 1, 8192 bytes) TCP: Hash tables configured (established 2048 bind 2048) UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. Unpacking initramfs... random: fast init done Freeing initrd memory: 11940K hw perfevents: enabled with armv7_cortex_a5 PMU driver, 3 counters available Initialise system trusted keyrings workingset: timestamp_bits=30 max_order=16 bucket_order=0 NFS: Registering the id_resolver key type Key type id_resolver registered Key type id_legacy registered nfs4filelayout_init: NFSv4 File Layout Driver Registering... jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc. Key type asymmetric registered Asymmetric key parser 'x509' registered io scheduler noop registered (default) io scheduler mq-deadline registered io scheduler kyber registered ADI serial driver adi-uart4.0: ttySC0 at MMIO 0x31003000 (irq = 20, base_baud = 7031250) is a ADI-UART4 console [ttySC0] enabled console [ttySC0] enabled bootconsole [earlycon0] disabled bootconsole [earlycon0] disabled loop: module loaded adi-spi3 31042000.spi: registered ADI SPI controller spi0 m25p80 spi2.38: unrecognized JEDEC id bytes: 9d, 60, 1a m25p80: probe of spi2.38 failed with error -2 adi-spi3 31044000.spi: registered ADI SPI controller spi2 libphy: Fixed MDIO Bus: probed adi-dwmac 3100c000.ethernet: PTP uses main clock adi-dwmac 3100c000.ethernet: no reset control found adi-dwmac 3100c000.ethernet: User ID: 0x10, Synopsys ID: 0x37 adi-dwmac 3100c000.ethernet: DWMAC1000 adi-dwmac 3100c000.ethernet: DMA HW capability register supported adi-dwmac 3100c000.ethernet: RX Checksum Offload Engine supported adi-dwmac 3100c000.ethernet: COE Type 2 adi-dwmac 3100c000.ethernet: TX Checksum insertion supported adi-dwmac 3100c000.ethernet: Wake-Up On Lan supported adi-dwmac 3100c000.ethernet: Enhanced/Alternate descriptors adi-dwmac 3100c000.ethernet: Enabled extended descriptors adi-dwmac 3100c000.ethernet: Ring mode enabled adi-dwmac 3100c000.ethernet: Enable RX Mitigation via HW Watchdog Timer libphy: stmmac: probed usbcore: registered new interface driver usb-storage musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected musb-hdrc musb-hdrc.3.auto: MUSB HDRC host driver musb-hdrc musb-hdrc.3.auto: new USB bus registered, assigned bus number 2 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected i2c /dev entries driver adi_wdt: initialized: timeout=20 sec (nowayout=0) Synopsys Designware Multimedia Card Interface Driver dwmmc_adi 31010000.mmc: IDMAC supports 32-bit address mode. dwmmc_adi 31010000.mmc: Using internal DMA controller. dwmmc_adi 31010000.mmc: Version ID is 270a dwmmc_adi 31010000.mmc: DW MMC controller at irq 38,32 bit host data width,1024 deep fifo mmc_host mmc0: Bus speed (slot 0) = 50000000Hz (slot req 400000Hz, actual 396825HZ div = 63) ADI hardware CRC crypto driver adi-hmac-crc 31001200.crc: initialized adi-hmac-crc 31001300.crc: initialized usbcore: registered new interface driver usbhid usbhid: USB HID core driver adau1761 0-0038: Direct firmware load for adau1761.bin failed with error -2 adau1761 0-0038: Could not find firmware file: -2 sc5xx-i2s-dai 31002000.i2s: SPORT create success snd-sc5xx scb:sound: adau-hifi <-> 31002000.i2s mapping ok NET: Registered protocol family 10 Segment Routing with IPv6 sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver NET: Registered protocol family 17 Key type dns_resolver registered ThumbEE CPU extension supported. Loading compiled-in X.509 certificates console [netcon0] enabled netconsole: network logging started TI DP83867 stmmac-0:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=stmmac-0:00, irq=POLL) adi-dwmac 3100c000.ethernet eth0: No Safety Features support found adi-dwmac 3100c000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported adi-dwmac 3100c000.ethernet eth0: registered PTP clock IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready adi-dwmac 3100c000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready IP-Config: Complete: device=eth0, hwaddr=02:80:ad:20:31:e2, ipaddr=10.99.24.96, mask=255.255.255.0, gw=10.99.24.1 host=sc58x, domain=, nis-domain=(none) bootserver=10.99.24.65, rootserver=10.99.24.65, rootpath= cfg80211: Loading compiled-in X.509 certificates for regulatory database cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' ALSA device list: #0: sc5xx-asoc-card platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 cfg80211: failed to load regulatory.db Freeing unused kernel memory: 1024K Run /init as init process init started: BusyBox v1.29.3 (2020-08-07 10:16:01 UTC) starting pid 665, tty '': '/bin/mount -t proc proc /proc' starting pid 666, tty '': '/bin/mount -t sysfs sysfs /sys' starting pid 667, tty '': '/bin/mount -t devtmpfs devtmpfs /dev' starting pid 668, tty '': '/bin/mount -o remount,rw /' starting pid 669, tty '': '/bin/mkdir -p /dev/pts' starting pid 670, tty '': '/bin/mount -t devpts devpts /dev/pts' starting pid 671, tty '': '/bin/mount -a' mount: mounting /dev/root on / failed: No such file or directory starting pid 675, tty '': '/usr/bin/fastboot-listener' Failed to open SHARC notify device: No such file or directory starting pid 678, tty '/dev/ttySC0': '/bin/sh'
There are more command available for USB in u-boot:
sc # usb info 1: Mass Storage, USB Revision 2.0 - Generic USB Storage 000000009451 - Class: (from Interface) Mass Storage - PacketSize: 64 Configurations: 1 - Vendor: 0x05e3 Product 0x0723 Version 148.81 Configuration: 1 - Interfaces: 1 Bus Powered 500mA Interface: 0 - Alternate Setting 0, Endpoints: 2 - Class Mass Storage, Transp. SCSI, Bulk only - Endpoint 1 In Bulk MaxPacket 512 - Endpoint 2 Out Bulk MaxPacket 512
sc # usb storage Device 0: Vendor: Generic Rev: 9451 Prod: STORAGE DEVICE Type: Removable Hard Disk Capacity: 1897.0 MB = 1.8 GB (3885056 x 512)
sc # usb tree USB device tree: 1 Mass Storage (12 Mb/s, 500mA) Generic USB Storage 000000009451
sc # fatinfo usb 0:1 Interface: USB Device 0: Vendor: Generic Rev: 9451 Prod: STORAGE DEVICE Type: Removable Hard Disk Capacity: 1897.0 MB = 1.8 GB (3885056 x 512) Filesystem: FAT32 " "
MACHINE | DTB_FILE | FULL_FS_IMAGE | MINIMAL_FS_IMAGE | RAMDISK_FILE |
---|---|---|---|---|
adsp-sc589-mini | sc589-mini.dtb | adsp-sc5xx-full-adsp-sc589-mini.tar.xz | adsp-sc5xx-minimal-adsp-sc589-mini.tar.xz | adsp-sc5xx-ramdisk-adsp-sc589-mini.cpio.xz.u-boot |
adsp-sc589-ezkit | sc589-ezkit.dtb | adsp-sc5xx-full-adsp-sc589-ezkit.tar.xz | adsp-sc5xx-minimal-adsp-sc589-ezkit.tar.xz | adsp-sc5xx-ramdisk-adsp-sc589-ezkit.cpio.xz.u-boot |
adsp-sc584-ezkit | sc584-ezkit.dtb | adsp-sc5xx-full-adsp-sc584-ezkit.tar.xz | adsp-sc5xx-minimal-adsp-sc584-ezkit.tar.xz | adsp-sc5xx-ramdisk-adsp-sc584-ezkit.cpio.xz.u-boot |
adsp-sc573-ezkit | sc573-ezkit.dtb | adsp-sc5xx-full-adsp-sc573-ezkit.tar.xz | adsp-sc5xx-minimal-adsp-sc573-ezkit.tar.xz | adsp-sc5xx-ramdisk-adsp-sc573-ezkit.cpio.xz.u-boot |