Ethernet driver provides driver for the MAC controller present in ADI processors. The ethernet driver package also has code to interface with the PHYs on the ADI released boards.
There are 2 network interfaces on ADSP-SC5xx : EMAC0 and EMAC1
U-Boot only supports one network port. You have to select one emac port in include/configs/sc589-ezkit.h at build time.(For SC584/SC573 EZ-Board , we should do it in file sc584-ezkit.h or sc573-ezkit.h)
#define CONFIG_DW_PORTS 1 // enable EMAC0 or #define CONFIG_DW_PORTS 2 // enable EMAC1
U-boot provides a set of basic net commands:
For example:
CPU: ADSP ADSP-SC589-0.0 (Detected Rev: 1.1) (spi flash boot) VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 225 MHz OCLK: 150 MHz I2C: ready DRAM: 112 MiB MMC: SC5XX SDH: 0 SF: Detected W25Q128BV with page size 256 Bytes, erase size 4 KiB, total 16 MiB In: serial Out: serial Err: serial other init Net: dwmac.3100c000 Hit any key to stop autoboot: 0 sc # sc # dhcp Speed: 100, full duplex BOOTP broadcast 1 BOOTP broadcast 2 DHCP client bound to address 10.99.24.200 (260 ms) sc # ping 10.99.24.94 Speed: 100, full duplex Using dwmac.3100c000 device host 10.99.24.94 is alive sc # tftp ${loadaddr} ${ramfile} Speed: 100, full duplex Using dwmac.3100c000 device TFTP from server 10.99.24.94; our IP address is 10.99.24.200 Filename 'uImage'. Load address: 0x89000000 Loading: ################################################################# ################################################################# ...... ##################################### 2 MiB/s done Bytes transferred = 10502080 (a03fc0 hex)