This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:platforms:microblaze [19 Jan 2018 10:11] – rename xcomm_zynq -> master Alexandru Ardelean | resources:tools-software:linux-drivers:platforms:microblaze [23 Apr 2018 11:33] – [Boot Kernel on FPGA Microblaze] Add XSDB support Istvan Csomortani | ||
---|---|---|---|
Line 158: | Line 158: | ||
==== Boot Kernel on FPGA Microblaze ==== | ==== Boot Kernel on FPGA Microblaze ==== | ||
- | Then one method to load the kernel onto the already built and running FPGA which has the Microblaze processor is to launch | + | Then one method to load the kernel onto the already built and running FPGA which has the Microblaze processor is to launch |
+ | |||
+ | <note important> | ||
< | < | ||
+ | xmd> fpga -f system_top.bit | ||
xmd> connect mb mdm | xmd> connect mb mdm | ||
xmd> dow simpleImage.vc707_fmcomms2-3 | xmd> dow simpleImage.vc707_fmcomms2-3 | ||
xmd> run | xmd> run | ||
+ | </ | ||
+ | |||
+ | < | ||
+ | xsdb> connect | ||
+ | xsdb> fpga -f system_top.bit | ||
+ | xsdb> targets | ||
+ | 1 xcku040 | ||
+ | | ||
+ | 3 MicroBlaze #0 (Running) | ||
+ | xsdb> targets 3 | ||
+ | xsdb> dow simpleImage.kcu105_fmcdaq2 | ||
+ | xsdb> con | ||
</ | </ | ||
(more details, methods of how to get bit file and kernel on flash and/or boot off SD Card is appreciated) | (more details, methods of how to get bit file and kernel on flash and/or boot off SD Card is appreciated) | ||