This is an old revision of the document!
This guide provides some step-by-step instructions on how to build a Microblaze Linux Kernel image for the FMC board connected to an
Microblaze gnu toolchain from Xilinx is no longer available on git. Please use gnu tools from SDK installation as below:
Dave@HAL9000:~/fmcomms1/linux$ export PATH=/opt/Xilinx/SDK/2015.2/gnu/microblaze/linux_toolchain/lin64_le/bin:$PATH
Dave@HAL9000:~/fmcomms1/linux$ export ARCH=microblaze
Dave@HAL9000:~/fmcomms1/linux$ export CROSS_COMPILE=microblazeel-xilinx-linux-gnu-
Download the Vivado SDK from here Download And make sure you followed the instructions for Microblaze GNU Toolchain
This specifies any shell prompt running on the development host
Dave@HAL9000:~$ git clone https://github.com/analogdevicesinc/linux.git Cloning into 'linux'... remote: Counting objects: 2757163, done. remote: Compressing objects: 100% (495484/495484), done. remote: Total 2757163 (delta 2296596), reused 2687337 (delta 2234506) Receiving objects: 100% (2757163/2757163), 782.04 MiB | 1.39 MiB/s, done. Resolving deltas: 100% (2296596/2296596), done. Dave@HAL9000:~$
This specifies any shell prompt running on the development host
Dave@HAL9000:~$ cd linux/ Dave@HAL9000:~/linux$ git checkout master Checking out files: 100% (16412/16412), done. Branch master set up to track remote branch master from origin. Switched to a new branch 'master' Dave@HAL9000:~/linux$
This specifies any shell prompt running on the development host
Dave@HAL9000:~/linux$ source /opt/Xilinx/SDK/2014.2/settings64.sh Dave@HAL9000:~/linux$ export ARCH=microblaze Dave@HAL9000:~/linux$ export CROSS_COMPILE=microblazeel-xilinx-linux-gnu-
This specifies any shell prompt running on the development host
Dave@HAL9000:~/linux$ make adi_mb_defconfig # # configuration written to .config # Dave@HAL9000:~/linux$
Root File-system (initramfs) rootfs.cpio.gz must be placed in the root of your kernel tree.
This specifies any shell prompt running on the target or development host
Dave@HAL9000:~/linux$ wget http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/rootfs.cpio.gz --2014-11-21 14:27:54-- http://wiki.analog.com/_media/resources/tools-software/linux-drivers/platforms/rootfs.cpio.gz Resolving wiki.analog.com (wiki.analog.com)... 195.170.124.184 Connecting to wiki.analog.com (wiki.analog.com)|195.170.124.184|:80... connected. HTTP request sent, awaiting response... 200 OK Length: 3006465 (2.9M) [application/octet-stream] Saving to: `rootfs.cpio.gz' 100%[===================================================================================================================================================================>] 3,006,465 75.1K/s in 37s 2014-11-21 14:28:32 (79.2 KB/s) - `rootfs.cpio.gz' saved [3006465/3006465] Dave@HAL9000:~/linux$
The result of building the kernel is an elf file in arch/microblaze/boot named simpleImage.<dts file name> based on the dts specified.
The build process for the kernel searches in the arch/microblaze/boot/dts directory for a specified device tree file and then builds the device tree into the kernel image.
The following command shows the general format for the build target name. Note that the <dts file name> does not include the file extension “.dts”.
Dave@HAL9000:~/linux$ make simpleImage.<dts file name>
To see what device-trees for the different FPGA carrier and FMC module combination exist type:
Dave@HAL9000:~/linux$ ls -l arch/microblaze/boot/dts
This specifies any shell prompt running on the target or development host
Dave@HAL9000:~/linux$ make -j4 simpleImage.kcu105_ad_fmcdaq2_ebz scripts/kconfig/conf --silentoldconfig Kconfig CHK include/config/kernel.release CHK include/generated/uapi/linux/version.h HOSTCC scripts/dtc/checks.o CC scripts/mod/empty.o [ --snip-- ] CC net/ipv4/xfrm4_output.o CC net/ipv4/xfrm4_protocol.o LD net/ipv4/built-in.o LD net/built-in.o LINK vmlinux LD vmlinux.o MODPOST vmlinux.o GEN .version CHK include/generated/compile.h UPD include/generated/compile.h CC init/version.o LD init/built-in.o KSYM .tmp_kallsyms1.o KSYM .tmp_kallsyms2.o LD vmlinux SORTEX vmlinux SYSMAP System.map CP vmlinux arch/microblaze/boot/simpleImage.kcu105_ad_fmcdaq2_ebz.unstrip OBJCOPY arch/microblaze/boot/simpleImage.kcu105_ad_fmcdaq2_ebz UIMAGE arch/microblaze/boot/simpleImage.kcu105_ad_fmcdaq2_ebz Image Name: Linux-3.17.0-126658-g6807aea Created: Thu Nov 20 16:50:28 2014 Image Type: MicroBlaze Linux Kernel Image (uncompressed) Data Size: 8425035 Bytes = 8227.57 kB = 8.03 MB Load Address: 80000000 Entry Point: 80000000 STRIP arch/microblaze/boot/simpleImage.kcu105_ad_fmcdaq2_ebz Kernel: arch/microblaze/boot/simpleImage.kcu105_ad_fmcdaq2_ebz is ready (#1642) Dave@HAL9000:~/linux$
Then one method to load the kernel onto the already built and running FPGA which has the Microblaze processor is to launch xmd from the xilinx vivado toolset from within …/linux/arch/microblaze/boot and run from the XMD shell:
xmd> connect mb mdm xmd> dow simpleImage.vc707_fmcomms2-3 xmd> run
(more details, methods of how to get bit file and kernel on flash and/or boot off SD Card is appreciated)