This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface Microwave converters. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Function | File |
---|---|
driver | drivers/iio/frequency/admv1014.c |
Documentation | Documentation/ABI/testing/sysfs-bus-iio |
Unlike PCI or USB devices, SPI devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each SPI bus segment, and what slave selects these devices are using. For this reason, the kernel code must instantiate SPI devices explicitly. The most common method is to declare the SPI devices by bus number.
This method is appropriate when the SPI bus is a system bus, as in many embedded systems, wherein each SPI bus has a number which is known in advance. It is thus possible to pre-declare the SPI devices that inhabit this bus. This is done with an array of struct spi_board_info, which is registered by calling spi_register_board_info().
For more information see: Documentation/spi/spi-summary.rst
compatible:
reg:
spi-max-frequency:
clocks:
clock-names:
clock-output-names:
clock-scales:
vcm-supply:
adi,parity-en:
adi,ibias-pd:
adi,if-amp-pd:
adi,quad-bg-pd:
adi,bb-amp-pd:
adi,quad-ibias-pd:
adi,det-en:
adi,bg-pd:
adi,p1db-comp:
adi,quad-se-mode:
adi,det-prog:
adi,adi,bb-amp-gain-ctrl:
'#address-cells':
'#size-cells':
'#clock-cells':
required:
spi { #address-cells = <1>; #size-cells = <0>; admv1014@0{ compatible = "adi,admv1014"; reg = <0>; spi-max-frequency = <1000000>; clocks = <&admv1014_lo>; clock-names = "lo_in"; clock-scales = <1 5>; vcm-supply = <&vcm>; adi,quad-se-mode = <12>; adi,parity-en; adi,det-en; adi,p1db-comp = <3>; adi,det-prog = <0>; adi,bb-amp-gain-ctrl = <0>; }; };
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The ADMV1014 Driver depends on CONFIG_SPI
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support Frequency ---> <*> Analog Devices ADMV1014 Microwave Downconverter
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 root:/sys/bus/iio/devices> iio:device0 root:/> ls -l -r--r--r-- 1 root root 4096 May 6 12:20 dev -r--r--r-- 1 root root 4096 May 6 12:20 name -rw-r--r-- 1 root root 4096 May 6 13:00 out_altvoltage0_i_hardwaregain -rw-r--r-- 1 root root 4096 May 6 13:00 out_altvoltage0_q_hardwaregain -rw-r--r-- 1 root root 4096 May 6 13:01 out_altvoltage0_i_offset -rw-r--r-- 1 root root 4096 May 6 13:01 out_altvoltage0_q_offset -rw-r--r-- 1 root root 4096 May 6 13:01 out_altvoltage0_i_phase -rw-r--r-- 1 root root 4096 May 6 13:01 out_altvoltage0_q_phase lrwxrwxrwx 1 root root 0 May 6 12:20 subsystem -> ../../../../../../../../bus/iio -rw-r--r-- 1 root root 4096 May 6 12:20 uevent
This specifies any shell prompt running on the target
root:/> cd /sys/bus/iio/devices/iio\:device0/ root:/> cat name admv1014
/sys/bus/iio/devices/iio:deviceX/out_altvoltageY_Z_hardwaregain
Gain factor. If shared across all channels, <type>_hardwaregain is used.
This specifies any shell prompt running on the target
root:/> cat out_altvoltage0_i_hardwaregain 0 0 root:/> echo 1.1 > out_altvoltage0_i_hardwaregain root:/> cat out_altvoltage0_hardwaregain 1 1
/sys/bus/iio/devices/iio:deviceX/out_altvoltageY_Z_offset
Offset value. If shared across all channels, <type>_offset is used.
This specifies any shell prompt running on the target
root:/> cat out_altvoltage0_i_offset 0 root:/> echo 1 > out_altvoltage0_i_offset root:/> cat out_altvoltage0_offset 1
/sys/bus/iio/devices/iio:deviceX/out_altvoltageY_Z_phase
Phase value. If shared across all channels, <type>_phase is used.
This specifies any shell prompt running on the target
root:/> cat out_altvoltage0_i_phase 0 root:/> echo 1 > out_altvoltage0_i_phase root:/> cat out_altvoltage0_phase 1