This is an old revision of the document!
The ADMFM2000 is a dual-channel microwave downconverter, system-in-package (SiP) module, with input RF and local oscillator (LO) frequency ranges covering 5 GHz to 32 GHz, with an output intermediate frequency (IF) frequency range from 0.5 GHz to 8 GHz. A common LO input signal is split to feed two separate buffer amplifiers to drive the mixer in each channel. Each down conversion path consists of an LNA, a mixer, an IF filter, a digital step attenuator (DSA), and an IF amplifier.
This driver supports the
This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface Microwave converters. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Source | Mainlined? |
---|---|
git | [In-progress] |
Function | File |
---|---|
driver | admfm2000.c |
device tree bindings | adi,admfm2000.yaml |
The ADMFM2000 driver is a platform driver and can currently only be instantiated via device tree.
Required properties:
Optional properties:
Example:
#include <dt-bindings/gpio/gpio.h> &{/} { admfm2000 { compatible = "adi,admfm2000"; switch1-gpios = <&gpio 1 GPIO_ACTIVE_LOW>, <&gpio 2 GPIO_ACTIVE_HIGH>; switch2-gpios = <&gpio 3 GPIO_ACTIVE_LOW>, <&gpio 4 GPIO_ACTIVE_HIGH>; attenuation1-gpios = <&gpio 17 GPIO_ACTIVE_LOW>, <&gpio 22 GPIO_ACTIVE_LOW>, <&gpio 23 GPIO_ACTIVE_LOW>, <&gpio 24 GPIO_ACTIVE_LOW>, <&gpio 25 GPIO_ACTIVE_LOW>; attenuation2-gpios = <&gpio 0 GPIO_ACTIVE_LOW>, <&gpio 5 GPIO_ACTIVE_LOW>, <&gpio 6 GPIO_ACTIVE_LOW>, <&gpio 16 GPIO_ACTIVE_LOW>, <&gpio 26 GPIO_ACTIVE_LOW>; #address-cells = <1>; #size-cells = <0>; channel@0 { reg = <0>; adi,direct-if-mode; }; channel@1 { reg = <1>; adi,direct-if-mode; }; }; };
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The ADMFM2000 driver depends on GPIOLIB
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support Frequency ---> <*> Analog Devices ADMFM2000 Dual Microwave Down Converter
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This device can be found under /sys/bus/iio/devices/
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 root:/sys/bus/iio/devices> cd iio:device0 root@analog:/sys/bus/iio/devices/iio:device0# ls -l total 0 -r--r--r-- 1 root root 4096 Oct 26 22:20 name lrwxrwxrwx 1 root root 0 Oct 26 22:20 of_node -> ../../../../firmware/devicetree/base/admfm2000 -rw-r--r-- 1 root root 4096 Oct 26 22:20 out_voltage0_hardwaregain -rw-r--r-- 1 root root 4096 Oct 26 22:20 out_voltage1_hardwaregain drwxr-xr-x 2 root root 0 Oct 26 22:20 power lrwxrwxrwx 1 root root 0 Oct 26 22:20 subsystem -> ../../../../bus/iio -rw-r--r-- 1 root root 4096 Oct 26 22:20 uevent -r--r--r-- 1 root root 4096 Oct 26 22:20 waiting_for_supplier root@analog:/sys/bus/iio/devices/iio:device0#
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device0# cat name admfm2000
/sys/bus/iio/devices/iio:deviceX/out_voltageY_hardwaregain
Hardware applied gain factor. If shared across all channels, <type>_hardwaregain is used.
This specifies any shell prompt running on the target
root@analog:/sys/bus/iio/devices/iio:device0#cat out_voltage0_hardwaregain -31.000000 dB root@analog:/sys/bus/iio/devices/iio:device0#echo -10 > out_voltage0_hardwaregain root@analog:/sys/bus/iio/devices/iio:device0#cat out_voltage0_hardwaregain -10.000000 dB