This is an old revision of the document!
This driver supports the
This is a Linux industrial I/O (IIO) subsystem driver, targeting multi-channel serial interface DACs. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Source | Mainlined? |
---|---|
git | [No] |
Required devicetree properties for the AD5770R:
Optional properties:
ad5770r@0 { compatible = "ad5770r"; reg = <0>; spi-max-frequency = <1000000>; vref-supply = <&vref>; reset-gpios = <&gpio 22 0>; channel@0 { num = <0>; adi,range-microamp = <0 300000>; }; channel@1 { num = <1>; adi,range-microamp = <0 140000>; }; channel@2 { num = <2>; adi,range-microamp = <0 55000>; }; channel@3 { num = <3>; adi,range-microamp = <0 45000>; }; channel@4 { num = <4>; adi,range-microamp = <0 45000>; }; channel@5 { num = <5>; adi,range-microamp = <0 45000>; }; }; vref: fixedregulator@0 { compatible = "regulator-fixed"; regulator-name = "fixed-supply"; regulator-min-microvolt = <1250000>; regulator-max-microvolt = <1250000>; };
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Device Drivers ---> ... <*> Industrial I/O support ---> --- Industrial I/O support ... Digital to analog converters ---> ... <*> Analog Devices AD5770R IDAC driver ... ... ...
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
This specifies any shell prompt running on the target
pi@raspberrypi:/sys/bus/iio/devices/iio:device0 $ cd /sys/bus/iio/devices/ pi@raspberrypi:/sys/bus/iio/devices $ ls iio:device0 iio:device1 pi@raspberrypi:/sys/bus/iio/devices $ cd iio\:device0 pi@raspberrypi:/sys/bus/iio/devices/iio:device0 $ ls -l total 0 -r--r--r-- 1 root root 4096 Jul 18 12:12 dev -r--r--r-- 1 root root 4096 Jul 18 12:12 name lrwxrwxrwx 1 root root 0 Jul 18 12:12 of_node -> ../../../../../../../../firmware/devicetree/base/soc/spi@7e204000/ad5770r@0 -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current0_filter_low_pass_3db_frequency -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current0_powerdown -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current0_raw -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current0_scale -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current1_filter_low_pass_3db_frequency -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current1_powerdown -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current1_raw -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current1_scale -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current2_filter_low_pass_3db_frequency -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current2_powerdown -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current2_raw -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current2_scale -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current3_filter_low_pass_3db_frequency -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current3_powerdown -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current3_raw -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current3_scale -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current4_filter_low_pass_3db_frequency -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current4_powerdown -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current4_raw -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current4_scale -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current5_filter_low_pass_3db_frequency -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current5_powerdown -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current5_raw -rw-r--r-- 1 root root 4096 Jul 18 12:12 out_current5_scale -r--r--r-- 1 root root 4096 Jul 18 12:12 out_current_filter_low_pass_3db_frequency_available drwxr-xr-x 2 root root 0 Jul 18 12:12 power lrwxrwxrwx 1 root root 0 Jul 18 12:12 subsystem -> ../../../../../../../../bus/iio -rw-r--r-- 1 root root 4096 Jul 18 12:12 uevent
This specifies any shell prompt running on the target
pi@raspberrypi:/sys/bus/iio/devices/iio:device0 $ cat name ad5770r
Description:
/sys/bus/iio/devices/iio:deviceX/out_currentY_scale
scale to be applied to out_currentY_raw in order to obtain the measured current in milliamps.
This specifies any shell prompt running on the target
root@raspberrypi:/sys/bus/iio/devices/iio:device0# cat out_current0_scale 0.018310546
Description:
/sys/bus/iio/devices/iio:deviceX/out_currentY_raw
Raw (unscaled, no bias etc.) output current for channel Y.
This specifies any shell prompt running on the target
root@raspberrypi:/sys/bus/iio/devices/iio:device0# echo 5000 > out_current0_raw
I = out_current0_raw * out_current0_scale = 5000 * 0,018310546 = 91,55273 mA
/sys/bus/iio/devices/iio:deviceX/out_currentY_powerdown
Description:
Writing 1 causes channel Y to enter power down mode. Clearing returns to
normal operation.
This specifies any shell prompt running on the target
root@raspberrypi:/sys/bus/iio/devices/iio:device0# echo 1 > out_current0_powerdown root@raspberrypi:/sys/bus/iio/devices/iio:device0# cat out_current0_powerdown 1 root@raspberrypi:/sys/bus/iio/devices/iio:device0# echo 0 > out_current0_powerdown root@raspberrypi:/sys/bus/iio/devices/iio:device0# cat out_current0_powerdown 0
/sys/bus/iio/devices/iio:deviceX/out_current_filter_low_pass_3db_frequency_available
Description:
Contains available filter frequencies.
This specifies any shell prompt running on the target
root@raspberrypi:/sys/bus/iio/devices/iio:device0# cat out_current_filter_low_pass_3db_frequency_available 153 357 715 1400 2800 262000
/sys/bus/iio/devices/iio:deviceX/out_current0_filter_low_pass_3db_frequency
Description:
Write filter value to channel Y.
This specifies any shell prompt running on the target
root@raspberrypi:/sys/bus/iio/devices/iio:device0# cat out_current0_filter_low_pass_3db_frequency 262000 root@raspberrypi:/sys/bus/iio/devices/iio:device0# echo 1000 > out_current0_filter_low_pass_3db_frequency root@raspberrypi:/sys/bus/iio/devices/iio:device0# cat out_current0_filter_low_pass_3db_frequency 1400