This is an old revision of the document!
This is a Linux industrial I/O (IIO) subsystem driver, targeting single and multi channel serial interface Capacitance to Digital Converters. The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc). See IIO for more information.
Source | Mainlined? |
---|---|
git | In Progress |
Function | File |
---|---|
driver | drivers/staging/iio/adc/ad7152.c |
Unlike PCI or USB devices, I2C devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each I2C bus segment, and what address these devices are using. For this reason, the kernel code must instantiate I2C devices explicitly. There are different ways to achieve this, depending on the context and requirements. However the most common method is to declare the I2C devices by bus number.
This method is appropriate when the I2C bus is a system bus, as in many embedded systems, wherein each I2C bus has a number which is known in advance. It is thus possible to pre-declare the I2C devices that inhabit this bus. This is done with an array of struct i2c_board_info, which is registered by calling i2c_register_board_info().
So, to enable such a driver one need only edit the board support file by adding an appropriate entry to i2c_board_info.
For more information see: Documentation/i2c/instantiating-devices.rst
Depending on the converter IC used, you may need to set the I2C_BOARD_INFO name accordingly, matching your part name.
ADI part number | I2C_BOARD_INFO Name |
---|---|
AD7152 | ad7152 |
AD7153 | ad7153 |
static struct i2c_board_info __initdata board_i2c_board_info[] = { #if defined(CONFIG_AD7152) || defined(CONFIG_AD7152_MODULE) { I2C_BOARD_INFO("ad7152", 0x48), }, #endif };
static int __init board_init(void) { [--snip--] i2c_register_board_info(0, board_i2c_board_info, ARRAY_SIZE(board_i2c_board_info)); [--snip--] return 0; } arch_initcall(board_init);
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Device Drivers ---> [*] Staging drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support [--snip--] *** Analog to digital converters *** <*> Analog Devices AD7152/3 capacitive sensor driver [--snip--]
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
<box 100% green|shell prompt running on the target>
root:/> cd /sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls iio:device0 root:/sys/bus/iio/devices> cd iio:device0 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> ls -l -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0-capacitance2_calibbias -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0-capacitance2_calibscale -r--r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0-capacitance2_raw -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0-capacitance2_scale -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0_calibbias --w------- 1 root root 4096 Jan 2 22:46 in_capacitance0_calibbias_calibration -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0_calibscale --w------- 1 root root 4096 Jan 2 22:46 in_capacitance0_calibscale_calibration -r--r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0_raw -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance0_scale -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1-capacitance3_calibbias -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1-capacitance3_calibscale -r--r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1-capacitance3_raw -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1-capacitance3_scale -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1_calibbias --w------- 1 root root 4096 Jan 2 22:46 in_capacitance1_calibbias_calibration -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1_calibscale --w------- 1 root root 4096 Jan 2 22:46 in_capacitance1_calibscale_calibration -r--r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1_raw -rw-r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance1_scale -r--r--r-- 1 root root 4096 Jan 2 22:46 in_capacitance_scale_available -r--r--r-- 1 root root 4096 Jan 2 22:46 name drwxr-xr-x 2 root root 0 Jan 2 22:46 power -rw-r--r-- 1 root root 4096 Jan 2 22:46 sampling_frequency -r--r--r-- 1 root root 4096 Jan 2 22:46 sampling_frequency_available lrwxrwxrwx 1 root root 0 Jan 2 22:46 subsystem -> ../../../../../../bus/iio -rw-r--r-- 1 root root 4096 Jan 2 22:46 uevent</box>
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat name ad7152</box>
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat sampling_frequency_available 200 50 20 17</box>
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat sampling_frequency 200 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> echo 50 > sampling_frequency root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat sampling_frequency 50 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0></box>
Lists all available scales for the input and input pairs:
ADC Input Pair | Channel name |
---|---|
CIN1(+) | in_capacitance0_raw |
CIN2(+) | in_capacitance1_raw |
CIN1(+) - CIN1(-) | in_capacitance0-capacitance2_raw |
CIN2(+) - CIN2(-) | in_capacitance1-capacitance3_raw |
Setting these directly influences the CDC input range, by altering the Input Range settings.
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance_scale_available 0.000061050 0.000030525 0.000015263 0.000007631</box>
Scale to be applied to in_capacitance0_raw, in_capacitance1_raw, in_capacitance0-capacitance2_raw and in_capacitance1-capacitance3_raw in order to obtain the measured capacitance in picofarads (pF). Allows the user to select one scale out of the available scales.
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance0_scale 0.000061050 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> echo 0.000030525 > in_capacitance0_scale root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance0_scale 0.000030525 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0></box>
Description:
Raw unscaled voltage measurement on channel in_capacitance0_raw
ADC Input Pair | Channel name |
---|---|
CIN1(+) | in_capacitance0_raw |
CIN2(+) | in_capacitance1_raw |
CIN1(+) - CIN1(-) | in_capacitance0-capacitance2_raw |
CIN2(+) - CIN2(-) | in_capacitance1-capacitance3_raw |
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance0_raw -1</box>
U = in_capacitance0_raw * in_capacitance0_scale = 23344 * 0.000030525 = 0.7126 pF
Description:
Raw unscaled voltage measurement on channel in_capacitance1-capacitance3_raw
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance1-capacitance3_raw -16</box>
U = in_capacitance1-capacitance3_raw * in_capacitance1-capacitance3_scale = -16 * 0.000030525 = -0.0004884 pF
Description:
Triggers gain calibration on channel in_capacitance0 or in_capacitance1
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> echo 1 > in_capacitance1_calibscale_calibration root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance1_calibscale 1.000000</box>
Description:
Write gain coefficient for channel in_capacitance0 or in_capacitance1
Valid range is between 1.0 and 1.99999999.
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> echo 1.5 > in_capacitance1_calibscale root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance1_calibscale 1.500000</box>
Description:
Triggers offset calibration on channel in_capacitance0 or in_capacitance1
<box 100% green|shell prompt running on the target>
root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> echo 1 > in_capacitance1_calibbias_calibration root:/sys/devices/platform/i2c-bfin-twi.0/i2c-0/0-0048/iio:device0> cat in_capacitance1_calibbias 12101</box>