Source | Mainlined? |
---|---|
git | [No] |
Function | File |
---|---|
driver | master/drivers/iio/adc/ad4630.c |
devicetree bindings | Documentation/devicetree/bindings/iio/adc/adi,ad4630.yaml |
devicetree for ad4630 | arch/arm/boot/dts/zynq-zed-adv7511-ad4630-24.dts |
devicetree for adaq4224 | arch/arm/boot/dts/zynq-zed-adv7511-adaq4224-24.dts |
The ad4030-24, ad4630-16, and ad4630-24 are 24-bit, 2 MSPS SAR ADCs highly configurable through an extensive configuration register list.
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
The AD4630 Driver depends on CONFIG_SPI
Linux Kernel Configuration Device Drivers ---> ... <*> Industrial I/O support ---> --- Industrial I/O support ... Analog to digital converters ---> ... <*> Analog Devices AD4630 ADC driver ... ... ...
// SPDX-License-Identifier: GPL-2.0
/*
* Analog Devices AD4630-24
*
* hdl_project: <ad4630_fmc/zed>
* board_revision: <B>
*
* Copyright (C) 2022 Analog Devices Inc.
*/
/dts-v1/;
#include "zynq-zed.dtsi"
#include "zynq-zed-adv7511.dtsi"
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/pwm/pwm.h>
/ {
vref: regulator-vref {
compatible = "regulator-fixed";
regulator-name = "fixed-supply";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
regulator-always-on;
};
vdd_1_8: regulator-vdd-1-8 {
compatible = "regulator-fixed";
regulator-name = "fixed-supply";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
vio: regulator-vio {
compatible = "regulator-fixed";
regulator-name = "fixed-supply";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
clocks {
cnv_ext_clk: ext-clk {
#clock-cells = <0x0>;
compatible = "fixed-clock";
clock-frequency = <100000000>;
clock-output-names = "cnv_ext_clk";
};
};
};
&fpga_axi {
rx_dma: rx-dmac@44a30000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x44a30000 0x1000>;
#dma-cells = <1>;
interrupts = <0 57 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clkc 15>;
adi,channels {
#size-cells = <0>;
#address-cells = <1>;
dma-channel@0 {
reg = <0>;
adi,source-bus-width = <64>;
adi,source-bus-type = <1>;
adi,destination-bus-width = <64>;
adi,destination-bus-type = <0>;
};
};
};
spi_clk: axi-clkgen@0x44a70000 {
compatible = "adi,axi-clkgen-2.00.a";
reg = <0x44a70000 0x10000>;
#clock-cells = <0>;
clocks = <&clkc 15>, <&clkc 15>;
clock-names = "s_axi_aclk", "clkin1";
clock-output-names = "spi_clk";
};
axi_pwm_gen: axi-pwm-gen@ {
compatible = "adi,axi-pwmgen";
reg = <0x44b00000 0x1000>;
label = "ad463x_cnv";
#pwm-cells = <2>;
clocks = <&cnv_ext_clk>;
};
axi_spi_engine: spi@44a00000 {
compatible = "adi,axi-spi-engine-1.00.a";
reg = <0x44a00000 0x1FF>;
interrupt-parent = <&intc>;
interrupts = <0 56 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clkc 15>, <&spi_clk>;
clock-names = "s_axi_aclk", "spi_clk";
num-cs = <1>;
#address-cells = <0x1>;
#size-cells = <0x0>;
ad463x: ad463x@0 {
compatible = "adi,ad463x";
reg = <0>;
vdd-supply = <&vref>;
vdd_1_8-supply = <&vdd_1_8>;
vio-supply = <&vio>;
vref-supply = <&vref>;
spi-max-frequency = <80000000>;
reset-gpios = <&gpio0 86 GPIO_ACTIVE_LOW>;
adi,lane-mode = <0>;
adi,clock-mode = <0>;
adi,out-data-mode = <0>;
adi,spi-trigger;
clocks = <&cnv_ext_clk>;
clock-names = "trigger_clock";
dmas = <&rx_dma 0>;
dma-names = "rx";
pwm-names = "spi_trigger", "cnv";
pwms = <&axi_pwm_gen 0 0>, <&axi_pwm_gen 1 0>;
};
};
};
Each and every IIO device, typically a hardware chip, has a device folder under /sys/bus/iio/devices/iio:deviceX. Where X is the IIO index of the device. Under every of these directory folders reside a set of files, depending on the characteristics and features of the hardware device in question. These files are consistently generalized and documented in the IIO ABI documentation. In order to determine which IIO deviceX corresponds to which hardware device, the user can read the name file /sys/bus/iio/devices/iio:deviceX/name. In case the sequence in which the iio device drivers are loaded/registered is constant, the numbering is constant and may be known in advance.
TIP: An example program whiroot@analog:/sys/bus/iio/devices# ls -lch uses the interface can be found here:
This specifies any shell prompt running on the target
root@analog:~ $ cat /sys/bus/iio/devices/iio\:device0/name adaq4224
Description:
Scale to be applied to in_voltageX_raw in order to obtain the measured voltage in millivolts
This specifies any shell prompt running on the target
root@analog:~ $ cat /sys/bus/iio/devices/iio\:device0/in_voltage0_scale 0.000196695
Description:
List of available scales to be applied to in_voltageX_raw in order to obtain the measured voltage in millivolts. This affects the gain applied to the input signal before ADC sampling. This attribute is available for ADAQ devices only.
This specifies any shell prompt running on the target
root@analog:~ $ cat /sys/bus/iio/devices/iio\:device0/in_voltage0_scale_available 0.000196695 0.000333786 0.001323223 0.003975629
Description:
Hardware applied calibration offset (calibbias). This is a hardware supported offset that can be applied to compensate for variation between different instances of the part.
This specifies any shell prompt running on the target
root@analog:~ $ cat /sys/bus/iio/devices/iio\:device0/in_voltage0_calibbias 0
Description:
Hardware applied calibration scale factor.
This specifies any shell prompt running on the target
root@analog:~ $ cat /sys/bus/iio/devices/iio\:device0/in_voltage0_calibscale 1.000000