Note: This section of the document applies to the ADSP-SC5xx (Cortex-A and SHARC+) and ADSPBF7xx processors. It does not apply to the ADuCM* processor families. CrossCore Embedded Studio provides support for the on-chip peripherals and EZ-KIT hosted device drivers that are provided for its processors. In order to use these features with FreeRTOS the source based versions of the drivers must be used rather than the default pre-built libraries that are provided.
To get started using UART alongside the FreeRTOS Add-In, you must first make sure that you have added the Pin Multiplexing and UART Add-Ins to your project. This should be automatically done by the Add-In when it is added to your project.
Now you should have both Pin Mulitplexing and the UART Add-Ins installed into your project.
This section is for removing UART functionality from an existing project. To remove UART we follow the inverse of the adding UART steps which are as follows.
Remove the source based version of the required services and driver: