This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:bfin:adas1000 [05 May 2016 18:18] – there was somehting funny re the zip file Catherine Redmond | resources:tools-software:bfin:adas1000 [05 May 2016 18:26] (current) – Catherine Redmond | ||
---|---|---|---|
Line 19: | Line 19: | ||
This project demonstrates a framework developed for Visual DSP [[adi> | This project demonstrates a framework developed for Visual DSP [[adi> | ||
- | {{ : | + | {{ : |
Line 28: | Line 28: | ||
* Display/ | * Display/ | ||
- | ==== Requirements: | + | ==== Requirements: |
- | * VisualDSP++ 5.0 Update 10 | + | * VisualDSP++ 5.0 Update 10 |
* [[adi> | * [[adi> | ||
- | * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++), | + | * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++), |
- | * Breakout board for SDP-B (If Hardware DRDY is used) [[adi> | + | * Breakout board for SDP-B (If Hardware DRDY is used) |
* ECG cables and simulator (if required) | * ECG cables and simulator (if required) | ||
Line 38: | Line 38: | ||
The attached zip file contains the relevant files for this project | The attached zip file contains the relevant files for this project | ||
- | {{: | ||
Zip File Contents & description: | Zip File Contents & description: | ||
Line 89: | Line 88: | ||
- Right click on the plot > Configure > Modify ' | - Right click on the plot > Configure > Modify ' | ||
- Halt the code, to see the latest ' | - Halt the code, to see the latest ' | ||
+ | ===== Zip file===== | ||
+ | {{: |