This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:bfin:adas1000 [12 Oct 2012 16:11] – created Catherine Redmond | resources:tools-software:bfin:adas1000 [05 May 2016 18:18] – there was somehting funny re the zip file Catherine Redmond | ||
---|---|---|---|
Line 9: | Line 9: | ||
===== Overview ===== | ===== Overview ===== | ||
- | The EVAL-ADAS1000SDZ is a fully featured evaluation kit for the ADAS1000. The evaluation kit consists of an evaluation board kitted with 2 ADAS1000 devices capable of demonstrating ECG capture up to 12 leads. | + | The EVAL-ADAS1000SDZ is a fully featured evaluation kit for the ADAS1000. The evaluation kit consists of an evaluation board kitted with 2 ADAS1000 devices capable of demonstrating ECG capture up to 12 leads. |
+ | This evaluation board is provided for silicon evaluation purposes and is not designed to be connected directly to animal or human. | ||
- | {{ : | + | This board can be operated in conjunction with the System Development Platform (SDP) or alternatively may be interfaced to directly via a dedicated serial interface connector (J4). |
+ | |||
+ | The SDP controller board connects to the PC via USB 2.0. The evaluation board connects to the SDP-B controller board. The [[adi> | ||
===== Framework Functional Description ===== | ===== Framework Functional Description ===== | ||
- | This project demonstrates a framework to interface ADAS1000 to ADSP-BF527 on SDP-B. | + | This project demonstrates a framework |
- | ==== The software | + | {{ : |
- | + | ||
- | * Configure various registers of ADAS1000 through SPORT1 of ADSP-BF527 | + | |
- | * Read ECG or Test tone data from ADAS1000 to memory of ADSP-BF527 (external SDRAM) | + | === The software |
- | * Process the data acquired from ADAS1000 | + | * Configure various registers of [[adi>ADAS1000]] through SPORT1 of [[adi> |
+ | * Read ECG or Test tone data from [[adi>ADAS1000]] to memory of [[adi> | ||
+ | * Process the data acquired from [[adi>ADAS1000]] | ||
* Display/ | * Display/ | ||
- | ===== Requirements: | + | ==== Requirements: |
+ | * VisualDSP++ 5.0 Update 10 | ||
+ | * [[adi> | ||
+ | * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++), | ||
+ | * Breakout board for SDP-B (If Hardware DRDY is used) [[adi> | ||
+ | * ECG cables and simulator (if required) | ||
- | * VisualDSP++ 5.0 Update 10 | + | ===== Framework Files ===== |
- | * ADAS1000 Eval Board setup, EVAL-ADAS1000SDZ | + | The attached zip file contains the relevant files for this project |
- | * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++) | + | |
- | * Breakout board for SDP-B (If Hardware DRDY is used) ADZS-BRKOUT-EX3 | + | |
- | * ECG cables and simulator (if required) | + | |
- | ===== Files: ===== | + | {{: |
+ | |||
+ | Zip File Contents & description: | ||
* ADAS1000_SDP_v1.c Main function which can be used to develop the application | * ADAS1000_SDP_v1.c Main function which can be used to develop the application | ||
* ADAS1K_Functions.c All the functions related to ADAS1000, which can be used by the application to read/write ADAS1000 registers, | * ADAS1K_Functions.c All the functions related to ADAS1000, which can be used by the application to read/write ADAS1000 registers, | ||
Line 39: | Line 48: | ||
* ADAS1000_SDP_v1.ldf Linker Description file, defining all the memory sections used by the processor | * ADAS1000_SDP_v1.ldf Linker Description file, defining all the memory sections used by the processor | ||
* ADAS1K_Functions.h Declaration of all functions related to ADAS1000, and Hardware DRDY pin definitions | * ADAS1K_Functions.h Declaration of all functions related to ADAS1000, and Hardware DRDY pin definitions | ||
- | * ADAS1K_RegValue.h Definitions of values for ADAS1000 registers which can be | + | * ADAS1K_RegValue.h Definitions of values for ADAS1000 registers which can be directly used during ADAS1000 register configuration. The values is calculated according to definitions in User_Config.h |
- | * directly used during ADAS1000 register configuration. The | + | * cdefADAS1K.h - Definitions of registers of ADAS1000, BIT Map, BIT Value and BIT Position definitions of all the fields of registers of ADAS1000 and other constant definitions and variable typdefs related to ADAS1000 |
- | * values is calculated according to definitions in | + | * cdefBF527_new.h - System MMR register addresses for PORT registers of BF527 Blackfin on SDP) |
- | * User_Config.h | + | * SPORT_Functions.h - Declaration of all the SPORT1 functions used for Serial Interface with ADAS1000 |
- | * cdefADAS1K.h - Definitions of registers of ADAS1000, BIT Map, BIT Value | + | * User_Config.h - All the user definable parameters for various functionalities of (ADAS1000 + SDP) system |
- | * and BIT Position definitions of all the fields of | + | |
- | * registers of ADAS1000 and other constant definitions and | + | |
- | * variable typdefs related to ADAS1000 | + | |
- | * cdefBF527_new.h - System MMR register addresses for PORT registers of BF527 | + | |
- | * (Blackfin on SDP) | + | |
- | * SPORT_Functions.h - Declaration of all the SPORT1 functions used for Serial | + | |
- | * Interface with ADAS1000 | + | |
- | * User_Config.h - All the user definable parameters for various | + | |
- | * functionalities of (ADAS1000 + SDP) system | + | |
- | + | ||
- | LA.vps - VDSP++ plot for LA data | + | |
- | LL.vps - VDSP++ plot for LL data | + | |
- | RA.vps - VDSP++ plot for RA data | + | |
- | V1.vps - VDSP++ plot for V1 data | + | |
- | V2.vps - VDSP++ plot for V2 data | + | |
- | + | ==== Implementation | |
- | ==== Implementation | + | |
* ' | * ' | ||
Line 70: | Line 68: | ||
* Initialize the data buffers (Input and processed data) | * Initialize the data buffers (Input and processed data) | ||
* In an infinite loop | * In an infinite loop | ||
- | * - Capture data frames from ADAS1000 | + | |
- | * - Process the captured frames | + | - Process the captured frames |
- | * - Display the processed data - TBD | + | - Display the processed data |
==== Procedure: ==== | ==== Procedure: ==== | ||
+ | === Hardware Setup === | ||
- | | + | |
- | - a) Connect J4 of SDP-B Rev 1.3 to J2 of ADAS1000 Eval board | + | - |
- | | + | - |
- | | + | - |
- | | + | - |
- | - 2) Open the project (ADAS1000_SDP_v1.dpj) in Visual DSP++ 5.0 Update 10 | + | - |
- | - 3) Modify UserConfig.h file for required operation | + | - |
- | - 4) Create and Connect to BF527 Emulator Session in Visual DSP++ | + | - |
- | - 5) Build the project | + | - |
- | - 6) Run the code. BF527 configures ADAS1000 and data is received continuously | + | - |
- | - from it. | + | - |
- | - 7) Plot the data | + | - |
- | - a) Menu > View > Debug Windows > Plot > Restore | + | - |
- | - b) Browse and open LA.vps and other plot files (.vps files) | + | - |
- | - c) Right click on the plot > Configure > Modify ' | + | |
- | - of samples | + | |
- | - 8) Halt the code, to see the latest ' | + | |
- | + | ||
- | ===== Framework fileset ===== | + | |
- | {{: | + | |