This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:ace:largecapture [05 Jul 2021 15:45] – Ciaran Watterson | resources:tools-software:ace:largecapture [03 Aug 2021 15:39] (current) – [Limitations and What to Expect] Ciaran Watterson | ||
---|---|---|---|
Line 9: | Line 9: | ||
<note important> | <note important> | ||
==== Limitations and What to Expect ==== | ==== Limitations and What to Expect ==== | ||
- | - The first limitation is the size of your paging file and amount of RAM your system has. | ||
- | - The FFT analysis library is limited to (2^31)-1 element double arrays. Note that Complex Samples are passed as an interleaved double array, the limitation for Complex FFTs is 2^30 I&Q samples. | ||
- Not all ACE plug-ins can support or have been updated to support large captures. | - Not all ACE plug-ins can support or have been updated to support large captures. | ||
+ | - The size of your paging file and amount of RAM your PC or Laptop has. | ||
+ | - Most Capture Controllers (e.g. ADS7-V2) take a snapshot to onboard RAM as the data rate is often too high to continuously transfer to the PC (reliably). For the SDP-H1 that's 64MB and the ADS7-V2 about 4GB. | ||
+ | - The FFT analysis library is limited to (2^31)-1 element double arrays. Note that Complex Samples are passed as an interleaved double array, the limitation for Complex FFTs is 2^30 I&Q samples. | ||
- Depending on the size of the Capture it could take a long time. | - Depending on the size of the Capture it could take a long time. | ||
- As the operation is memory intensive some applications may stop responding or your system may become unstable. | - As the operation is memory intensive some applications may stop responding or your system may become unstable. |