This shows you the differences between two versions of the page.
resources:pmods:ad5160 [28 Sep 2012 16:12] – created Dragos Bogdan | resources:pmods:ad5160 [29 May 2013 10:59] (current) – grammar error Lucian Sin | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | The [[adi> | + | The [[adi> |
The wiper settings are controllable through an SPI-compatible digital interface. The resistance between the wiper and either end point of the fixed resistor varies linearly with respect to the digital code transferred into the RDAC latch. | The wiper settings are controllable through an SPI-compatible digital interface. The resistance between the wiper and either end point of the fixed resistor varies linearly with respect to the digital code transferred into the RDAC latch. |