This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [10 Dec 2012 15:57] – Download Wrapper Alexandru.Tofan | resources:fpga:xilinx:pmod:adxrs453_adxl345_lx9 [09 Jan 2021 00:57] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 4: | Line 4: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://www.xilinx.com/products/ | + | * [[xilinx>products/ |
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
Line 15: | Line 15: | ||
==== Running Demo (SDK) Program ==== | ==== Running Demo (SDK) Program ==== | ||
- | <note tip>If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[http://www.xilinx.com/products/ | + | <WRAP round 80% tip> |
- | </note> | + | \\ |
+ | If you are not familiar with LX9 and/or Xilix tools, please visit\\ [[xilinx>products/ | ||
+ | </WRAP> | ||
- | To begin, connect the PmodGYRO2 to J5 connector of LX9 board, pins 7 to 12 (see image below). You must use an extension cable or the [[http:// | + | To begin, connect the PmodGYRO2 to J5 connector of LX9 board, pins 7 to 12. You must use an extension cable or the [[http:// |
{{: | {{: | ||
Line 32: | Line 34: | ||
On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | On the LX-9 MicroBoard D10 and D9 display the Tap/Double Tap status. If you tap the device once, D10 will turn on for a short period of time. If you double tap the device, D10 and D9 will both turn on at the same time.\\ | ||
- | <note important> | + | <WRAP round 80% important> |
* Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | * Connecting the PmodGYRO2 must be done with an extension cable or a PmodTPH. | ||
* Connecting the PmodACL to the board with an extension cable provides ease of use. | * Connecting the PmodACL to the board with an extension cable provides ease of use. | ||
* UART must be set to 57600 baudrate. | * UART must be set to 57600 baudrate. | ||
- | </note> | + | </WRAP> |
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
+ | \\ | ||
{{: | {{: | ||
</ | </ |