This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:fpga:xilinx:interposer:terminal_common [02 Jul 2013 12:02] – Correct typeos Istvan Csomortani | resources:fpga:xilinx:interposer:terminal_common [02 Jul 2013 13:58] (current) – Add title ++Upload Application Software++ Istvan Csomortani | ||
---|---|---|---|
Line 22: | Line 22: | ||
{{ : | {{ : | ||
+ | |||
+ | ===== Upload Application Software ===== | ||
After the configuration of the terminal was finished, the software application has to be uploaded and started on the configured system. This can be done by running the // | After the configuration of the terminal was finished, the software application has to be uploaded and started on the configured system. This can be done by running the // | ||
<WRAP tip>If the script threw an error, verify if the Xilinx EDK path specified in the **Loadapp.bat** script is corresponding with the current install path. If not change it to the correct one.</ | <WRAP tip>If the script threw an error, verify if the Xilinx EDK path specified in the **Loadapp.bat** script is corresponding with the current install path. If not change it to the correct one.</ |