This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:import_workspace [13 Aug 2013 09:22] – created Lucian Sin | resources:fpga:xilinx:interposer:import_workspace [30 Sep 2013 10:30] – added information about uncomment the device name from comm. file Lucian Sin | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | The **HDL Reference Design** for each supported Xilinx FPGA board contains a folder called | + | The **HDL Reference Design** for each supported Xilinx FPGA board contains a folder called **SDK_Workspace** which stores the Xilinx SDK project files needed to build the no-OS software and also the .bit files with the HDL design that must be programmed into the FPGA. |
These are the steps that need to be followed to recreate the software project: | These are the steps that need to be followed to recreate the software project: | ||
- | * Download | + | * First download |
- | {{: | + | {{: |
+ | | ||
+ | {{: | ||
+ | * In SDK folder you'll find the **SDK_Workspace** folder. Make sure that the path where it is stored does not contain any spaces. | ||
* Open the Xilinx SDK. When the SDK starts, it asks you to provide a folder where to store the workspace. Any folder can be provided. | * Open the Xilinx SDK. When the SDK starts, it asks you to provide a folder where to store the workspace. Any folder can be provided. | ||
* In the SDK select the // | * In the SDK select the // | ||
Line 8: | Line 11: | ||
* In the //Import// window select the // | * In the //Import// window select the // | ||
{{: | {{: | ||
- | * In the //Import Projects// window select the //**SDK_Workspace**// folder as root directory. After the root directory is chosen the projects that reside in that directory will appear in the // | + | * In the //Import Projects// window select the **SDK_Workspace** folder as root directory. After the root directory is chosen the projects that reside in that directory will appear in the // |
{{: | {{: | ||
- | * The //Project Explorer// window now shows the projects that exist in the workspace and the files for each project. The SDK should automatically build the projects and the //Console// window will display the result of the build. If the build is not done automatically, | + | * The //Project Explorer// window now shows the projects that exist in the workspace |
- | {{: | + | {{: |
- | * At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. | + | * Now the software must be added in your project. For downloading the software, you must use 3 links from Github given in **Downloads** section. From there you'll download the specific driver, the specific commands |
+ | {{: | ||
+ | |||
+ | <WRAP round important 80%> | ||
+ | * Before compilation you have to uncomment the name of the device that you currently use. In the picture below there is an example of this, which works only with AD5629R project. For another device, uncomment only the respective name. You can have one driver working on multiple devices, so the drivers' | ||
+ | </ | ||
+ | {{: | ||
+ | * The SDK should automatically build the projects and the //Console// window will display the result of the build. If the build is not done automatically, |