Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revisionBoth sides next revision
resources:fpga:xilinx:interposer:ad9834 [28 May 2012 15:53] – Approved Alexandru.Tofanresources:fpga:xilinx:interposer:ad9834 [28 Sep 2012 13:19] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costina
Line 16: Line 16:
 {{ :resources:fpga:xilinx:interposer:img_ad9834.jpg }} {{ :resources:fpga:xilinx:interposer:img_ad9834.jpg }}
  
-For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to Analog Devices [[/resources/eval/sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: +{{page>common_sdp}}
-  * a controller board, like the **[[resources/eval/sdp/sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** +
-  * a compatible Analog Devices SDP [[adi>sdp#exallist|product evaluation board]] +
-  * corresponding PC software +
-The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software.  Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ.+
  
 Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD9834SDZ** Evaluation Board. Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD9834SDZ** Evaluation Board.
resources/fpga/xilinx/interposer/ad9834.txt · Last modified: 09 Jan 2021 00:49 by Robin Getz