This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5541a [29 Jul 2013 17:12] – changed source code (without using Micrium uC-Probe) Lucian Sin | resources:fpga:xilinx:interposer:ad5541a [06 Sep 2013 15:50] – added link to EDK KC705 reference project on Github Lucian Sin | ||
---|---|---|---|
Line 39: | Line 39: | ||
* [[http:// | * [[http:// | ||
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
- | * **EVAL-AD5541A** evaluation board | + | * **EVAL-AD5541ASDZ** evaluation board |
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 14.6 (Programmer IMPACT is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
* UART Terminal (Termite/ | * UART Terminal (Termite/ | ||
- | * The EVAL-AD5541ASDZ | + | * The EVAL-AD5541A |
- | + | ||
- | <WRAP round info 80%> | + | |
- | The EVAL-AD5541ASDZ reference project for Xilinx KC705 FPGA consists of three parts: the **AD5541A Driver**, | + | |
- | + | ||
- | All three parts have to be downloaded. | + | |
- | </ | + | |
===== Downloads ===== | ===== Downloads ===== | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
- | | + | \\ |
- | * **AD5541A Driver: | + | |
- | * **EVAL-AD5541ASDZ Demo for Xilinx KC705 FPGA: ** https:// | + | * **AD5541A Driver:** https:// |
- | * **Xilinx | + | * **AD5541A Commands:** https:// |
+ | * **Xilinx | ||
+ | * **EDK KC705 Reference project:** https:// | ||
+ | \\ | ||
</ | </ | ||
- | |||
- | |||
====== Run the Demonstration Project ====== | ====== Run the Demonstration Project ====== | ||
+ | |||
===== Hardware setup ===== | ===== Hardware setup ===== | ||
Line 72: | Line 68: | ||
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
* Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
- | * Start IMPACT, and double click “Boundary Scan”. Right click and select Initialize Chain. The program should recognize the Kintex 7 device (see screenshot below). | ||
- | {{ : | ||
- | * Program the KC705 FPGA using the ”download.bit” file provided in downloads section. | ||
- | * Power the ADI evaluation board. | ||
- | ==== Reference Project Overview ==== | + | ===== Quick start evaluation ===== |
- | The following commands were implemented in this version of EVAL-AD5541ASDZ | + | For a quick start evaluation, run the **download.bat** script located in the **SDK/ |
+ | |||
+ | <WRAP round info 80%> | ||
+ | \\ | ||
+ | The **download.bat** script assumes that the Xilinx ISE Design Suite 14.6 is installed at this path: **C:/ | ||
+ | </ | ||
+ | |||
+ | If programming was successful, you should be seeing the command messages appear on the terminal. | ||
+ | ===== Reference Project Overview | ||
+ | The following commands were implemented in this version of EVAL-AD5541A | ||
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| **help?** | Displays all available commands. | | | **help?** | Displays all available commands. | | ||
Line 91: | Line 92: | ||
{{ : | {{ : | ||
+ | ===== Software Project Setup ===== | ||
+ | {{page> | ||
====== More information ====== | ====== More information ====== | ||
* [[resources: | * [[resources: | ||
{{page> | {{page> |