Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:peripherals:spi_engine:engine [25 Mar 2015 17:28] – [Configuration Parameters] Lars-Peter Clausenresources:fpga:peripherals:spi_engine:engine [04 Sep 2019 12:44] (current) – Fix source links and some grammar mistakes Istvan Csomortani
Line 1: Line 1:
-====== SPI-Engine Execution FPGA Peripheral ======+====== SPI Engine Execution FPGA Peripheral ======
  
 {{ :resources:fpga:peripherals:spi_engine:spi_engine_execution.png|}} {{ :resources:fpga:peripherals:spi_engine:spi_engine_execution.png|}}
  
-The SPI-Engine Execution peripheral forms the heart of the SPI-Engine framework. It is responsible for handling a SPI-Engine control stream and translate it into low-level SPI bus transactions.+The SPI Engine Execution peripheral forms the heart of the SPI Engine framework. It is responsible for handling a SPI Engine control stream and translates it into low-level SPI bus transactions.
  
 ===== Files ===== ===== Files =====
  
 ^ Name ^ Description ^ ^ Name ^ Description ^
-| .v | Verilog source for the peripheral. | +[[github>hdl?master/library/spi_engine/spi_engine_execution/spi_engine_execution.v|spi_engine_execution.v]] | Verilog source for the peripheral. | 
-| .tcl | TCL script to generate the Vivado IP-integrator project for the peripheral. |+[[github>hdl?master/library/spi_engine/spi_engine_execution/spi_engine_execution_ip.tcl|spi_engine_execution_ip.tcl]] | TCL script to generate the Vivado IP-integrator project for the peripheral. |
  
 ===== Configuration Parameters ===== ===== Configuration Parameters =====
  
 ^ Name ^ Description ^ Default ^ ^ Name ^ Description ^ Default ^
-| ''NUM_CS'' | Number of chip-select signals for the SPI bus (min: 1, max: 8) | 1 +| ''NUM_CS'' | Number of chip-select signals for the SPI bus (min: 1, max: 8) | 1 | 
 +| ''DEFAULT_SPI_CFG'' | Reset configuration value for the [[.:instruction_format#spi_configuration_register|SPI configuration register]] | 0 | 
 +| ''DEFAULT_CLK_DIV'' | Reset configuration value for the [[.:instruction_format#prescaler_configuration_register|prescaler clock divider register]] | 0 | 
 +| ''DATA_WIDTH'' | Data width of the parallel data stream. Will define the transaction's granularity. Supported values: 8/16/24/32| 8 | 
 +| ''NUM_OF_SDI'' | Number of multiple SDI lines, (min: 1, max: 8) | 1 |
  
 ===== Signal and Interface Pins ===== ===== Signal and Interface Pins =====
Line 21: Line 24:
 ^ Name ^ Type ^ Description ^ ^ Name ^ Type ^ Description ^
 | ''clk'' | Clock | All other signals are synchronous to this clock. | | ''clk'' | Clock | All other signals are synchronous to this clock. |
-| ''resetn'' | Synchronous active low reset | Resets the internal state machine of the core. |+| ''resetn'' | Synchronous active-low reset | Resets the internal state machine of the core. |
 | ''active'' | Output | Indicates whether the peripheral is currently active and processing commands. | | ''active'' | Output | Indicates whether the peripheral is currently active and processing commands. |
-| ''ctrl'' | [[SPI-Engine Control Interface]] slave | SPI-Engine Control stream that contains commands and data for the execution module. |+| ''ctrl'' | [[SPI Engine Control Interface]] slave | SPI Engine Control stream that contains commands and data for the execution module. |
 | ''spi'' | [[SPI bus interface]] master | Low-level SPI bus interface that is controlled by peripheral. | | ''spi'' | [[SPI bus interface]] master | Low-level SPI bus interface that is controlled by peripheral. |
  
 ===== Theory of Operation ===== ===== Theory of Operation =====
  
-The ''active'' signal is be asserted as long as the peripheral is busy executing incoming commands.+The SPI Engine Execution module implements the physical access to the SPI bus. It implements a small but powerful programmable state machine that translates a SPI Engine command stream into low-level SPI bus access.  
 + 
 +Communication with a command stream generator happens via the ''ctrl'' interface and the low-level SPI access is handled on the ''spi'' interface. The ''active'' signal is asserted as long as the peripheral is busy executing incoming commands. 
 + 
 +Internally the SPI Engine execution module consists of an instruction encoder that translates the incoming commands into an internal control signal, a multi-function counter and compares unit that is responsible for handling the timing and a shift register which holds the received and transmitted SPI data. 
 + 
 +The module has an optional programmable pre-scaler register that can be used to divide the external clock to the counter and compare unit. 
 + 
 +{{:resources:fpga:peripherals:spi_engine:spi_engine.svg|}} 
 +===== More Information ===== 
 +  * [[.|SPI Engine Framework]]
resources/fpga/peripherals/spi_engine/engine.1427300886.txt.gz · Last modified: 25 Mar 2015 17:28 by Lars-Peter Clausen