This is an old revision of the document!
The DAC JESD204B/C Transport Peripheral (AD-IP-JESD204-TRANSPORT-DAC) implements the transport level handling of a JESD204B/C transmitter device. It is compatible with a wide range of Analog Devices high-speed digital-to-analog converters.
The core handles the JESD204B/C framing of the user-provided payload data. In addition it is capable of generating standard and user-defined test-pattern data for interface verification. It also features a per-channel dual-tone DDS that can be used to dynamically generate test-tones.
The peripheral can be configured at runtime through a AXI4-Lite memory mapped register map.
Name | Description | Default |
---|---|---|
ID | Instance identification number. | 0 |
NUM_LANES | Number of lanes supported by the peripheral. Equivalent to JESD204 L parameter. | 4 |
NUM_CHANNELS | Number of converters supported by the peripheral. Equivalent to JESD204 M parameter. | 2 |
SAMPLES_PER_FRAME | Number of samples per frame. Equivalent to JESD204 S parameter. | 1 |
CONVERTER_RESOLUTION | Resolution of the converter. Equivalent to JESD204 N parameter. | 16 |
BITS_PER_SAMPLE | Number of bits per sample. Equivalent to JESD204 NP parameter. | 16 |
OCTETS_PER_BEAT | Number of bytes per beat for each link. | 4 |
DDS_TYPE | DDS Type. Set 1 for CORDIC or 2 for Polynomial | 1 |
DDS_CORDIC_DW | CORDIC DDS Data Width | 16 |
DDS_CORDIC_PHASE_DW | CORDIC DDS Phase Width | 16 |
DATAPATH_DISABLE | Disable instantiation of DDS core. | 0 |
Name | Type | Description |
---|---|---|
Configuration interface | ||
s_axi_aclk | Clock | All S_AXI signals and irq are synchronous to this clock. |
s_axi_aresetn | Synchronous active low reset | Resets the internal state of the peripheral. |
S_AXI | AXI4-Lite bus slave | Memory mapped AXI-lite bus that provides access to modules register map. |
Link layer interface | ||
link_clk | Clock | Device clock for the JESD204B/C interface. Must be line clock / 40 for 204B correct operation. Must be line clock / 66 for correct 204C operation. |
LINK_DATA | AXI4-Streaming interface | Framed transmit data towards link layer. |
Application layer interface | ||
enable | Output | Request signal for each channel. |
dac_valid | Output | Qualifier signal for each channel. Always '1'. |
dac_ddata | Input | Raw application layer data, every channel concatenated. |
dac_dunf | Input | Application layer underflow. |
The data is intended for the DAC can have multiple sources:
The application layer connects to the framer block when the DMA source is selected. The framer module takes sample data and maps it onto the format that the JESD204 link expects for the specified framer configuration.
The data in the application layer interface dac_ddata
is expected to have the following layout:
MSB LSB [ MmSn, ..., MmS1, MnS0, ..., M1Sn, ... M1S1, M1S0, M0Sn, ... M0S1, M0S0 ]
Where MjSi refers to the i-th sample of the j-th converter. With m being the number of converters and n the number of samples per converter per beat.
The core asserts the enable
signal for each channel that is enabled by the software. The dac_ddata
data bus must contain data for each channel regardless if the channels are enabled or not.
The link layer interface description can be found in the User Data Interface section of the JESD204B/C Link Transmit Peripheral IP.
The REG_STATUS
(0x054
) register CLK_FREQ
field allows to determine the clock rate of the device clock (link_clk
) relative to the AXI interface clock (s_axi_aclk
). This can be used to verify that the device clock is running at the expected rate.
The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock this corresponds to a resolution of 1.523kHz per LSB. A raw value of 0 indicates that the link clock is currently not active.
By setting the EXT_SYNC parameter of the IP an external synchronization signal dac_sync_in
can be used to trigger data movement from user application layer to the link layer, reset internal DDS cores or PRBS generators.
The external synchronization signal should be synchronous with the dac clock. Synchronization will be done on the rising edge of the signal.
The self clearing SYNC
control bit from the REG_CNTRL_1
(0x44
) register will arm the trigger logic to wait for the external sync signal. The DAC_SYNC_STATUS
status bit from the REG_SYNC_STATUS
(0x68
) register will show that the synchronization is armed but the synchronization signal has not yet been received.
Once the sync signal is received the data will start to flow and the DAC_SYNC_STATUS
status bit will reflect that with a deassertion.
Reduced number of octets-per-frame (F
) settings. The following values are supported by the peripheral: 1, 2, 4
Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the EngineerZone.