This is an old revision of the document!
The 7 Series and Ultrascale FPGAs Transceivers Wizard can be used to configure the transceivers inside the util_adxcvr core. In general in all reference designs the gigabit transceivers are configured to the highest supported line rate of the device. If the user wants to use their system with a different line rate, she needs to reconfigure the transceivers. This can be done by software, which does the reconfiguration through the DRP interface of the transceivers. Due the complexity of the transceivers, it can happen that the user needs to do addition settings in HDL using the Wizard. The following wiki provides a short guide on how to use the wizard to generate a transceiver configuration for a JESD204B interface.
The following features are required for a JESD204B interface:
The first one is using the GT wizard manually as explained below: Using_the_GUI_of_the_Wizard, and a second one that uses a script to generate one or more configurations: Using_the_generator_script. Please keep in mind that the script is capable of generating only configurations where the TX ad RX lane rates are even.
Regardless of the methon you are using, there is a script that parses the generated configurations and generates a list containing only the parameters that are different from the default, therefor the ones that you will have to change/add in your system_bd.tcl: Parsing_script. In the manual flow, you will also have to call the parsing script manually, but in the other one it is called implicitly.
To start the wizard in the Vivado, a project should be loaded with a 7 Series FPGA which has gigabit transceivers. In the Project Manager select IP catalog and search after the keyword wizard, then select the 7 Series FPGAs Transceivers Wizard IP.
You can define a custom name for your component and leave it on default. The tools should recognize your transceiver type automatically, if not, you may have to double check if you have the right FPGA device selected for your project. You also need to select Include Shared Logic in core at the Shared Logic section in order to have both COMMON and CHANNEL instances in the generated code.
First, you need to select JESD204 as targeted protocol and specify your line rate and reference clock. A valid reference clock depends on your line rate. Make sure that you're using a valid reference clock form the drop-down list. Also you should set the used PLLs for TX and RX. If your line rate is equal for both directions, you can use the same PLL. Be aware that each PLL's VCO has a different frequency range where the circuit can function correctly. If your targeted line rate is too high or too low, you may be restricted to use just one of the two PLLs. All other settings can be left on their default value in this tab.
If you selected JESD204 to be the used protocol, you don't have to change anything here. The JESD204B interface is using 8B/10B encoding/decoding, and the internal data width will be 40 bits. In all the reference designs the DRP frequency is connected to the system clock (100 MHz). In the Synchronization and Clocking section, both TX and RX should have an enabled buffer. The PLLREFCLK is used as the source for TXOUTCLK and RXOUTCLK.
The setting from the tabs PCIe, SATA, PRBS and CB and CC Sequence can be left to their default values.
Location of the COMMON instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/<component_name>_common.v Location of the CHANNEL instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/<component_name>_gt.v
[~] less daq2_zc706.srcs/sources_1/ip/gtwizard_0/gtwizard_0_common.v [~] less daq2_zc706.srcs/sources_1/ip/gtwizard_0/gtwizard_0_gt.v
This instances should be compared with the COMMON and CHANNEL instances used in util_adxcvr_cm.v and util_adxcvr_ch.v.
The overall workflow with the Ultrascale FPGAs Transceiver Wizard is similar to the 7 Series one, it just has a different GUI. To open up the wizard in the Project Manager select IP Catalog and search after the keyword wizard, then select the Ultrascale FPGAs Transceivers Wizard. You can define a custom name for your component and leave it on default. The tools should recognize your transceiver type automatically, if not, you may have to double check if you have the right FPGA device selected for your project. To apply the general JESD204B setting, select the GTH-JESD204 preset. In the first tab, called Basic you can find all the necessary settings. Select the targeted line rate, PLL and reference clock. The tool will tell you what PLL and reference clock can be used with a specific line rate. Note that the current version of the util_adxcvr core does not support QPLL Fractional-N option.
To have both COMMON and CHANNEL instances inside the generated core, in the Structural Options tab the Include transceiver COMMON in the Core option must be selected.
To find the actual instance attributes, two different files should be examined. A generic one, which contains the actual software macro instance, and a wrapper, which instanciates the previous file and sets the required attributes.
Location of the COMMON instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/gtwizard_ultrascale_v1_7_gthe4_common.v
Location of the COMMON wrapper: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/<component_name>_gthe4_common_wrapper.v
Location of the CHANNEL instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/gtwizard_ultrascale_v1_7_gthe4_channel.v
Location of the CHANNEL instance: <project_name>/<project_name>.srcs/sources_1/ip/<component_name>/synth/<component_name>_gthe4_channel_wrapper.v
[~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gtwizard_ultrascale_v1_7_gthe4_common.v [~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gth_jesd204_gthe4_common_wrapper.v [~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gtwizard_ultrascale_v1_7_gthe4_channel.v [~] less daq2_zcu102.srcs/sources_1/ip/gth_jesd204/synth/gth_jesd204_gthe4_channel_wrapper.v
This generated attributes values should be compared with the values used with the COMMON and CHANNEL instances in util_adxcvr_cm.v and util_adxcvr_ch.v.
Open the TCL console inside your Vivado project. Source gtwizard_generator.tcl
source ../../scripts/gtwizard_generator.tcl
Call the get_diff_params method with the desired parameters.
get_diff_params 15.4 QPLL0 385
The first parameter represents the lane rate that will be set to both rx and tx. The second one can be CPLL, QPLL0, QPLL1. The third one is the reference clock. If left empty, then it will be filled with all the viable values for the lane rate given.
get_diff_params {9.8304} QPLL0 {} false
The fourth parameter is optional. If you set it to false, the script will remove from the project and delete from disk the generated IPs after the list of parameters is done, so you don't have to do that manually.
Both the first and the third parameters are actually lists, so you can use that to generate multiple configurations. Keep in mind that the script will generate IPs with all the combinations between the lane rate and reference clock.
get_diff_params {9.8304 4.9152} QPLL0 {245.76 122.88} false
This call makes 4 instances of trancievers, and also deletes them after generating the list becouse of the 4th parameter is set to false.
Now, you should find the files at <project_name>.gen/sources_1/ip Make sure to overwrite the list from system_bd with the one in <GT_Type>_cfng.txt.
If you used the script to generate the IP, there is no need to call this one again, since it has already been called inside the get_diff_params method.
If you used the manual flow, make sure that you generated output products for the tranciever before going forward.
Navigate to <project_name>.gen/sources_1/ip Call gtwiz_parser.pl <GT_Type>. Check the files for the needed parameters. If you run the script wile having multiple configurations, it will include the unique ones for each IP, plus the gt_global list that contains the common parameters within generated configurations that are different from the default values. Make sure to overwrite the list from system_bd with the one in <GT_Type>_cfng.txt.